Contact us

Uma nova janela será aberta Uma nova janela será aberta

Motor Drivers

Toshiba has over 35 years of experience in the fabrication of motor drivers. These are used for various applications, including industrial equipment such as industrial sewing machines and automatic teller machines (ATMs), home appliances such as air conditioners and refrigerators, and office equipment such as printers and scanners. Toshiba offers an extensive portfolio of motor drivers suitable for the control of brushed DC motors, brushless DC motors and stepping motors. Owing to its unique motor drive technology, Toshiba motor drivers deliver high drive efficiency. Furthermore, these are housed in small packages due to the use of a new analog process. Therefore, they help achieve stable motor control and reduce system size and power consumption.
Product List

Motor Drivers Product Lineup (Parametric Search)
Search for motor drivers that best suit your needs.

  

Automotive Motor Drivers

thumb_car

Application Examples

thumb_motor_1

Downloading PSpice® models

pspice-img
Downloading PSpice® models
[Download Flow]
  1. Click on the 'Go to the Agreement page' button below and read the terms of use for the PSpice® models. If you accept all the terms, select the 'Yes' radio button and click the button 'I understand and agree'.
  2. This will take you to the online registration form. Fill in the form. Confirm that all the data are correct, and click the 'Send' button.
  3. You will receive an on-screen confirmation message acknowledging that your registration has been accepted. You will thereafter receive download information at your registered email address.
  4. Click on the URL embedded in the email and download the desired PSpice® models.

    PSpice® models are provided as zip-compressed files.
    To run a simulation, you need to prepare a PSpice® simulation environment.
    PSpice is a registered trademark of Cadence Design Systems, Inc.

Go to the Agreement page.

Motor Drivers with PSpice models list (2019/3/15 update)
  • Brushed motor drivers
    TB62216, TB6552, TB6569, TB6643, TB67H301, TB67H303, TB67H400A, TB67H452, TB67Z800, TC78H610, TC78H620, TC78H611, TC78H630
  • Brushless motor drivers
    TB6575, TB6585, TC78B002, TC78B006, TC78B006B, TC78B016, TB67B054
  • Stepping motor drivers
    TB62214A, TB62218A, TB6600, TB67S101A, TB67S109A, TB67S149, TB67S158, TB67S179, TB67S269, TB67S508, TC78S122, TB67S209, TC78H621, TC78H630, TC78H651, TB67S111

Introduction of Evaluation Boards


 

Downloading reference designs

Frequently Asked Questions

Cross Reference Search

  • Cross-reference search is a search service which offers you suitable Toshiba products from other manufacturers' products.

Contatos

Se você tiver alguma dúvida, clique em um destes links:

Dúvidas técnicas
Dúvidas sobre compras, exemplos e confiabilidade de IC
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.