Contact us

Uma nova janela será aberta Uma nova janela será aberta

SDHC Memory Card with Wireless LAN

Related Information

Catalog | Memory Microsite | Memory Blog

Product Number: THNSW008GAA-B(QB6)

The THNSW008GAA-B(QB6) is an SDHC memory card with wireless LAN functionality.
This SDHC memory card has a built-in Wi-Fi access point and a Web server function. Thus, files held in the card can be easily accessed by using either a Web browser or an app. Alternatively, files can also be accessed by issuing a CGI command from an external wireless LAN device such as a PC or a smartphone to the built-in Web server. Because the card functions as a wireless access point on its own, it can be used at any place where no 3G communication network or Wi-Fi access point is available.

You can develop your own apps*1 or set up your own configuration to adapt the card for various devices. Visit the FlashAir Developers site for information on app development.
https://www.flashair-developers.com/

The card is compliant with the iSDIO standard; thus, its wireless LAN functionality can be controlled from the host.
For details of the iSDIO standard, visit the website of the SD Association.
http://www.sdcard.org



  • *1: Although the THNSW008GAA-B(QB6) has the same hardware configuration as the Toshiba FlashAir™, FlashAir apps released by Toshiba cannot be used for this SDHC memory card.
SDHC Memory Card with Wireless LAN

The THNSW008GAA-B(QB6) has no label on the front side; you can affix your own label.
The wireless certificate numbers and other information are imprinted on the back side. The certificate numbers in Japan, the USA, Canada and European countries are already imprinted.
For certification of other countries, territories or regions, please contact the Toshiba engineering department.
To sell the card in countries, territories or regions where it is not certified, you will need to apply for certification.

Key Specifications

Product number THNSW008GAA-B(QB6)
Capacity 8 GB (7.2-GB user area)
Speed Class Class 10
Standard Compliance SD memory card standard, Version 4.00 / iSDIO standard
Wireless LAN Standard IEEE802.11b/g/n
Wireless Security WEP, TKIP, AES (WPA, WPA2)
Outline Dimensions 32.0 mm (L) × 24.0 mm (W) × 2.1 mm (T)
Countries/Territories Where the Card Is Certified Japan, USA, Canada, Taiwan, Hong Kong, Australia, New Zealand, Germany, France, Italy, Belgium, Netherlands, Luxemburg, United Kingdom, Ireland, Denmark, Greece, Spain, Portugal, Austria, Sweden, Finland, Estonia, Latvia, Lithuania, Poland, Czech, Slovakia, Hungary, Slovenia, Malta, Cyprus, Bulgaria, Romania, Switzerland, Norway, Liechtenstein, Iceland, Singapore, India, Indonesia, Philippines, South Korea, Vietnam, South Africa, Russia

Contatos

Se você tiver alguma dúvida, clique em um destes links:

Dúvidas técnicas
Dúvidas sobre compras, exemplos e confiabilidade de IC
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.