Contact us

Uma nova janela será aberta Uma nova janela será aberta

I2S (Inter-IC Sound)

I2S is a serial interface which transfers audio data. The following way is utilized to play music using recorded data in storage media such as an audio CD or a USB memory. At first, digital data are read from the storage media. And the data are transferred to a decoder IC which extracts music data. The music data is sent to a DA converter IC and converted to analog signals to play the music. I2S interface is adopted to transfer the music data from the decoder IC to the DA converter IC.

i2s_e

Product List

TX03 series products incorporating an I2S interface are displayed.

Contatos

Se você tiver alguma dúvida, clique em um destes links:

Dúvidas técnicas
Dúvidas sobre compras, exemplos e confiabilidade de IC
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.