Contact us

Uma nova janela será aberta Uma nova janela será aberta

Radio-Frequency Devices

Variable Capacitance Diodes Mais

These diodes have the capacities variable depending on the value of the reverse bias voltage applied between the anode and the cathode. They are also called VCDs (Variable Capacitance Diodes) or VariCaps. They are used in radio-frequency matching circuits for electronic tuning.

Radio-Frequency Switching Diodes Mais

They are particularly optimum for switching UHF/VHF frequency band of TV tuners.

Radio-Frequency Schottky Barrier Diodes Mais

Making use of rectifying property brought about by contact of a metal and a semiconductor, in place of P-N junction, these diodes are activated by a majority carrier. They are suitable for radio-frequency signal mixer circuits because the forward voltage is low and the reverse recovery time is short.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.