Contact us

Откроется новое окно Откроется новое окно

What is the definition of “allowable power dissipation”?

The allowable power dissipation is the maximum power dissipation permitted at up to the rated maximum junction temperature (Tj) of 150℃ when the ambient temperature, Ta, is 25℃. User should calcurate the derated allowable power dissipation because it should be decreased for higher ambient temperature.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.