Contact us

在新視窗打開 在新視窗打開

TOSHIBA推出高讀取密集型企業級SAS 固態硬碟PX04SL系列

January 19, 2016

適用資料倉儲、網路伺服器、媒體串流與隨選視訊

一次滿足企業用戶多重使用需求!

TOSHIBA_eSSD_PX04SL

【2016年1月19日-台北訊】硬碟機領導品牌台灣東芝電子零組件股份有限公司於今天宣布推出高讀取密集型企業級SAS固態硬碟PX04SL系列,此款產品專為資料倉儲、網路伺服器、媒體串流與隨選視訊(VOD)等需密集型讀取的應用工作設計,達到工作負荷最佳化!

TOSHIBA PX04SL系列是PX04S世代中最具有成本效益的解決方案,提供2TB[1] 及4TB兩種容量,將可在不犧牲效能的前提下,協助組織與企業用戶大幅降低總體持有成本(TCO)。不僅如此,此款具有270K IOPS[2] 的持續隨機讀取效能,不僅如此,此款具有270K IOPS  的持續隨機讀取效能,使用者將能感受到讀取密集的應用工作負荷達到絕佳的效果!。而在解決瓶頸方面,此款PX04SL SAS 固態硬碟則可為有效的資料吞吐量提供高密度的儲存,以達成在最大應用可擴充性上的高效能、高可靠性與耐久度等三大亮點。台灣東芝電子零組件股份有限公司儲存裝置事業部總經理坂上直表示:「我們相信全新加入的第三代PX04SL系列,將能充分展現TOSHIBA在固態硬碟穩定成長的市場中獨具的垂直整合與領導力。」TOSHIBA PX04SL 企業級SAS固態硬碟系列今正式上市。

Notes:

[1] 容量定義:Toshiba的定義為1MB等於1,000,000位元組、1GB等於1,000,000,000位元組、1TB等於1,000,000,000,000位元組。不過電腦作業系統回報儲存容量時是以2次方為單位,其定義為1GB = 230 = 1,073,741,824位元組,因此其顯示的容量較低。可用儲存容量(包括各種媒體檔案範例)會根據檔案大小、格式、設定、軟體與微軟作業系統等作業系統與/或是先安裝之應用軟體、或媒體內容等因素而有所不同。實際格式化後的容量可能有所差異。

[2] 讀寫速度根據主機裝置、讀寫條件與檔案大小而有所不同。

Customer Inquiries:

台灣東芝電子零組件股份有限公司

Tel: +886-2-2508-9988

Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.

·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.