If the packages are the same, are the thermal resistances the same?

Even if the packages are the same, the thermal resistances are not always the same.
Thermal resistance varies depending on chip size and internal structure, too.

If the package is the same but the thermal resistance is different, even if the same power dissipation occurs, the junction temperature of the semiconductor device is different.

開啟新視窗