How to calculate thermal resistance of diodes?

The junction-to-ambient thermal resistance, Rth(j-a), of a small-signal diode can be calculated from its power dissipation as follows:

Equation: Rth(j-a) = (Tj Max - Ta) / P Max

The thermal resistance can be calculated from its power dissipation  in the technical datasheet of the diodes.
The following is the formula for calculating the thermal resistance from the junction to the ambient.

Equation: Rth(j-a) = (Tj Max - Ta) / P Max

Rth(j-a): Junction-to-ambient thermal resistance
Tj Max: Maximum junction temperature
Ta: Ambient temperature (temperature condition of P Max)
P Max: Maximum power dissipation

Related Links

For products, please refer to the following links.

開啟新視窗