What is the purpose of the capacitor connected to one of the external resistors for an adjustable-output LDO?

feedback capacitor

The output voltage of an adjustable-output LDO is programmable via two resistors. The capacitor connected to the upper resistor (R1) is called a feedback capacitor (CFB). It is added to prevent oscillation, improve load transient response, and increase the ripple rejection ratio (R.R.) (also known as the power supply rejection ratio or PSRR for short). CFB and R1 introduce a zero and thus provide lead phase compensation, increasing an oscillation margin and improving load transient response.

To view the lineup of adjustable-output LDOs to which a feedback capacitor (CFB) can be connected, click:

For other LDO regulators, visit the main web page of LDO regulators at:

開啟新視窗