What is an output discharge function of the load switch IC?

Figure 1 Example of the VOUT waveform of a load switch IC with an output discharge function
Figure 1 Example of the VOUT waveform of a load switch IC with an output discharge function

The output discharge function brings the VOUT voltage to the GND level when the output of a load switch IC is disabled. When the load switch IC is disabled, the  output discharge function turns on the internal MOSFET between VOUT and GND, quickly discharging the capacitor connected to the VOUT terminal. This function is necessary for the proper operation of advanced electronic systems requiring exact power sequencing for various circuits, microprocessor units (MPUs), and other ICs.

Please also refer to the following documents for related explanations.

Application note

To product list of load switch ICs :

Main web page about load switch ICs

Other information

開啟新視窗