How should unused terminals of bus switches and analog switches be handled?

Unused pins (I/O pins) of bus switches and analog switches can be left open. The control pin needs pull-up/pull-down.

It is recommended, however, to pull up or down the I/O pins that are exposed to large external noise or other disturbances. In this case, the pull-up and pull-down resistors on the input and output sides of a switch should have the same value to make their voltages equal in order to prevent unnecessary current flow.

Related Links

The following documents also contain related information.

FAQs

Product Lists

Application Notes

開啟新視窗