Contact us

在新視窗打開 在新視窗打開

Function to suppress inrush current

When the output is turned on, the charging current flows through the output capacitor. If this current is too large, the overcurrent protection circuit may malfunction, making it impossible to start up, or the output voltage may overshoot. This function restricts the current flowing through the output capacitor to prevent this. Toshiba eFuse IC can reduce the inrush current by using an adjustable slew rate control function with an external capacitance.

Function to suppress inrush current

The larger the output capacitor and the higher the input voltage, the higher the inrush current. This large inrush current may cause failure. In that case, it is effective to keep the inrush current low by the slew rate control function.Our eFuse IC can adjust the slew rate of the output voltage with a small external capacitance, which simplifies the design of circuits that suppress the inrush current.

聯繫方式

如您需查詢,請點擊其中任何一個連結

技術方面的問題
購買、樣片和IC可靠性的相關諮詢
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.