Contact us

在新視窗打開 在新視窗打開

High-precision overvoltage clamp function

The overvoltage clamp function limits the output voltage to the limit voltage when the limit voltage is exceeded. Toshiba eFuse IC has a function to prevent excessive voltage from being applied to the ICs at subsequent stages by clamping the output voltage to the specified output voltage of individual products.

High-precision overvoltage clamp function

Our eFuse IC has an overvoltage clamping function. For example, in the case of the TCK805, even if the input voltage increases, the input voltage is suppressed to the about 6.0-V (typ.). Therefore, even if the input voltage instantaneously becomes excessive, more stable power supply can be provided by keeping the output voltage with this clamp function and keeping it within the withstand voltage of the post-stage IC.

聯繫方式

如您需查詢,請點擊其中任何一個連結

技術方面的問題
購買、樣片和IC可靠性的相關諮詢
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.