Uninterruptible Power Supply (UPS) Solution

Improving power supply performance and protection function contributes to energy saving and stable operation
Uninterruptible Power Supply (UPS) Solution

Uninterruptible power supplies (UPSs) are necessary for the continued operation of equipment in the event of a power failure. By supplying power that was normally charged from commercial power to the battery, the equipment can be safely shut down, backed up, and protected when power failure happens by typhoons and lightning strikes for example. Power supply failures cause equipment failure, data loss, file collapse, etc., and the restoration of these system failures requires enormous time and expense. In addition, network system shutdowns can lead to not only physical damage, but also losing of business opportunities and credibility. UPS are indispensable to prevent such situations. In recent years, prices are cheper, and users who record video on high-capacity HDDs at all times, players of online games, and individual online traders are becoming increasingly familiar. High-efficiency performance is strongly required for large-capacity types, while small-and medium-capacity types also require performance such as compactness and light weight. Toshiba's MOSFET having new process technology with a high heat dissipation package, contributes to the realization of a highly efficient power supply, and offering performances suitable for power supply circuitry and output stages of equipment. To maintain stable operation in harsh environments, Toshiba's photocouplers can be used to solve problems.

Features

  • MOSFETs’ improvement of power utilization efficiency by reducing on-resistance
  • MOSFETs’ high heat dissipation package for reduction of heat generation
  • Optical coupling provides high isolation strength and improves signal line operational stability
  • Compliance with safety standards (UL, cUL, etc.) (photocouplers)
  • Useful application notes, reference designs, and other documents on the web save design cycle time

Bi-directional DC-DC Converter

DC-AC inverter

Other block diagrams

USB block Protection circuit
Example of ESD protection circuit for USB signal line
Application / Uninterruptible Power Supply
RS-232 block Protection circuit
Example of ESD protection circuit for RS-232C signal line
Application / Uninterruptible Power Supply
Display block Protection circuit
Example of ESD protection circuit for a display signal line
Application / Uninterruptible Power Supply
DCDC – MCU DC signal transmission line
Example of signal transmission circuit between MCU and DC-DC
Application / Uninterruptible Power Supply
Digital signal Transmission line
Example of MCU digital signal transmission circuit
Application / Uninterruptible Power Supply
Analog signal Transmission line
Example of signal transmission circuit between power supply line and analog front end
Application / Uninterruptible Power Supply
The motion analysis (Power supply)
Example of power factor improvement circuit using PFC converter
Application / Uninterruptible Power Supply
For power supply DC-DC converter (Power supply)
Example of signal transmission circuit between control MCU and DC-DC converter for power supply
Application / Uninterruptible Power Supply
For output DC-DC converter (Power supply)
Example of signal transmission circuit between control MCU and DC-DC converter for output
Application / Uninterruptible Power Supply
The motion analysis (Battery charger)
Application / Uninterruptible Power Supply
For power supply DC-DC converter (Battery charger)
Application / Uninterruptible Power Supply
For output DC-DC converter (Battery charger)
Application / Uninterruptible Power Supply

Other Technical Content

Blood glucose meter solution
Realize high precision measurement and low power consumption in a small size
Surveillance Camera Solutions
Increasing demand of Functions and High resolution video
Programmable Logic Controller (PLC) Solution
Contributes to energy saving and stable operation by improving power supply performance and protective functions
Thermostat Solutions
Contributes to Product miniaturization, Long-life operation and Improvement of Quality and Reliability
Air Cleaner Solutions
Cleans Dirty Air by Linking "Filtration" with High-performance Filters and IoT
IoT sensor solutions
Ultra-low power consumption with high precision sensing in small size
Electric Toothbrush Solution
How to Obtain Oral Care that cannot be achieved by Human Hands?
Wireless Earphone Solution
For Long Time Operation with a Small Battery on a Wireless Earphone
Semiconductor Solutions for Air Conditioners
How to Increase Air Conditioning Performance without Increasing Power Consumption?
Smart Speaker Solution
Towards home network hub adding displays and cameras
Semiconductor Solutions for Servers
Contribute to Energy Saving and Stable Operation by Improving Power Supply Performance and Protective Functions
SSD Solution
Towards achievement compact size, high reliability and long life
Smartwatch Solution
To Realize More Features, Longer Operating Time and Smaller Size
Cordless Power Tool Solution
To Realize Compact, Light, Easy-to-Carry and Easy-to-Work with Long Time Operation

* Company names, product names, and service names may be trademarks of their respective companies.

開啟新視窗