型號查詢

交叉搜尋

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

關鍵字搜尋

參數搜尋

線上庫存查詢跟購買

Select Product Categories

The output voltage from a CMOS logic IC alternates between High and Low for a certain period of time. That is, the output goes into oscillation. What can I do to prevent this?

Major causes include the following:

  1. A slowly changing input signal might exceed the specified input rise and fall times.Ensure that the input signal meets the input rise and fall times specified in the datasheet, or use a Schmitt-trigger input type.
  2. The power supply or GND might not be stable. In this case, stabilize the power supply, for example, by using a bypass capacitor. For power supply stabilization, please refer to “Is a decoupling capacitor required between VCC and GND?” in the Frequently Asked Questions (FAQ) page.
  3. An input signal might have noise. Use a lowpass filter to filter out noise from the input signal. If the use of a lowpass filter makes it impossible to meet the input rise and fall times specifications, use a Schmitt-trigger input type.
開啟新視窗