型號查詢

交叉搜尋

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

關鍵字搜尋

參數搜尋

線上庫存查詢跟購買

Select Product Categories

Features of the Toshiba Motor Driver ICs Fabricated with the state-of-the-art 0.13-μm process, Toshiba's motor driver ICs help improve motor performance.

Industry's first motor driver ICs fabricated with the state-of-the-art 0.13-μm BiCD/CD process

In order to develop motor driver ICs that will help reduce the power consumption and acoustic noise of motor applications, it is necessary to improve the speed and performance of AD converters and power transistors and to increase logic integration density. However, it is not practical to try to address all these needs using conventional technologies because doing so will cause the die size to increase and thus impact the overall cost.
Instead, Toshiba has adopted the state-of-the-art BiCD/CD process, an industry-leading 0.13-μm high-voltage mixed-signal process with the world's lowest on-resistance (RonA). Thanks to the significant increase in circuit density, new driver ICs will help improve motor performance with smaller footprints and lower costs and thus meet exacting customer needs.

Safety features for improving the motor reliability

Since 1980, Toshiba has accumulated over 30 years of experience in the development of motor driver ICs. Toshiba has continuously led the industry, establishing a highly successful track record. During this period, Toshiba has used each new generation of processes to enhance performance and add new features for ensuring smooth and quiet motor operation. Toshiba has continued to improve the IC performance. Recent additions to our product portfolio include motor driver ICs with various safety features for detecting abnormal conditions, such as overcurrent, overtemperature and faulty behavior. These ICs contribute to improving the motor reliability. Furthermore, Toshiba has been integrating peripheral circuit functions onto the same chip to reduce the external parts count and thus the overall cost.

Over 100 motor driver ICs to meet a wide range of needs

To meet a wide range of market needs, Toshiba offers over 100 motor driver ICs for brushless motor, stepping motor and brushed motor applications. Our product portfolio includes many motor driver ICs that are specifically designed to address the market's growing needs, such as sine-wave driver ICs for air-conditioner fan motor applications that integrate an IPD and the controller section of a motor driver in a system-in-package (SiP) and single-chip driver ICs for small fan motor applications in refrigerators, ventilators, etc. Additionally, Toshiba is actively developing new motor driver ICs to expand its product portfolio.

Setting a new trend for the industry

Toshiba will continue to use the state-of-the-art process to increase the levels of integration, improve performance, reduce size and cut costs. At the same time, Toshiba stays in close contact with its customers to better understand their needs and respond to them in a timely fashion.
Moreover, Toshiba will cooperate with the Corporate Manufacturing Engineering Center, which is involved in the R&D of electrical motors to actively offer new proposals for improving motor performance and to develop new trend-setting and industry-leading technologies.

500V/2A Sine-Wave Motor Driver ICs

TB67B000HG
One package (MCD+IPD)

Single-Chip Motor Driver ICs for Small Fan Applications

TC78B002FTG
A new window will open