型號查詢

交叉搜尋

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

關鍵字搜尋

參數搜尋

線上庫存查詢跟購買

Select Product Categories

Image Recognition Processors Visconti™: Roadmap and System Organizations

Roadmap

This is a roadmap of the TMPV75 and TMPV76 series of image recognition processors.

The Visconti™5 (TMPV770) series of artificial intelligence (AI) processors for automotive image recognition incorporating deep neural network (DNN) hardware IP will be available for sampling in September 2019. The Visconti™5 series is suitable for advanced driver assistance system (ADAS) and automatic driving applications.
Toshiba has been developing image recognition processors since the 1990s and released a test chip in 2001. After making further improvements, we released a first-generation product, the Visconti™ (T5BG3XBG), in 2003.
In 2011, Toshiba released the Visconti2 (TMPV750) Series that incorporates not only a suite of image processing accelerators optimized for human recognition but also a new enhancement that allows the use of color cameras to detect both brightness and color. In 2013, Toshiba launched the Visconti3 (TMPV752) Series that contains two instances of Arm® Cortex®-A9 MPCore with single- and double-precision floating-point units (FPUs).

This is a roadmap of the Advanced Driver Assistance Systems and Euro NCAP Requirements.

In November 2014, exploiting pattern recognition using luminance-based and color-based image information, the Visconti4 (TMPV760) Series delivers a significant improvement in image recognition at nighttime. Additionally, the Visconti4 (TMPV760) Series allows 3D reconstruction using the input stream of a monocular camera and can detect standstill obstacles on the road surface.

Basic System Organizations

Visconti4 TMPV7608XBG

This is the basic system configuration example of image recognition processor (TMPV7608XBG).
* The video input interface of the TMPV7608XBG has a 4-of-8 video switch.

Lineup

View the product list of image recognition processors to find products that meet your performance specifications.

* MIPI is a registered trademark owned by the MIPI Alliance.
* Microsoft and Windows are either registered trademarks or trademarks of Microsoft Corporation in the United States and/or other countries.
* Red Hat and Enterprise Linux are registered trademarks of Red Hat, Inc. in the United States and other countries.
* HDMI is a trademark or registered trademark of HDMI Licensing, LLC in the United States and/or other countries.
* MediaLB and MOST are registered trademarks of Microchip Technology Inc. in the United States and other countries.
* Arm and Cortex are registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
* All other company names, product names, and service names mentioned herein may be trademarks of their respective companies.

聯繫我們

技術方面問題

聯絡我們

聯絡我們

常見問題

常見問答

Queries about purchasing, sampling and IC reliability

線上庫存查詢跟購買

keyword:

開啟新視窗