require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Company about
June 17, 2014
Feature Low Drop-out Voltage, Low Output Noise Voltage, Low Inrush Current
IRVINE , Calif., — Toshiba America Electronic Components, Inc. (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today announced two new additions to its TCR3D series of 300mA single output CMOS-LDO regulator ICs. The new TCR3DMxx is housed in a small DFN4 (1.0x1.0x0.58mm) package; and the TCR3DFxx comes in a general purpose SMV(SOT-25)(2.8x2.9x1.1mm) package.
Both feature low drop-out voltage, low output noise voltage and a built-in low inrush current reduction circuit.
Toshiba offers more than 40 products with a fixed output voltage ranging from 1.0 to 4.5V to accommodate various applications , including smart phones, tablet PCs, portable audio players, digital cameras, game consoles and other small mobile devices.
CMOS-LDO regulators enable a low profile, low supply current and low dropout, making them a popular power management choice for mobile devices. Toshiba's micro CMOS process helps the regulators improve the tradeoff between characteristics and size. A small package size makes the new LDO regulators suitable for applications requiring high-density packaging, such as portable devices.
Series | Output current | Output voltage | Package | Inrush current reduction | Thermal shut down | Output auto-discharge | Number of output voltage types |
TCR3DMxx | 300mA | 1.0 to 4.5V | DFN4 | ✓ | ✓ | ✓ | 15 |
TCR3DFxx | 300mA | 1.0 to 4.5V | DFN4 | ✓ | ✓ | ✓ | 28 |
Toshiba's new 300mA CMOS-LDO regulator ICs are available now. Budgetary pricing is $0.05-$0.07. Please contact your local Toshiba Sales Office for samples and pricing.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today's leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's sixth largest semiconductor manufacturer (Gartner, 2013 Worldwide Semiconductor Revenue, December 2013). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 590 consolidated companies employing over 200,000 people worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.
For additional company and product information, please visit http://www.toshiba.com/taec/.
Product density is identified based on the density of memory chip(s) within the Product, not the amount of memory capacity available for data storage by the end user. Consumer-usable capacity will be less due to overhead data areas, formatting, bad blocks, and other constraints, and may also vary based on the host device and application. For details, please refer to applicable product specifications
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.
LGSS 14 713