Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Keyword Search

Parametric Search

Stock Check & Purchase

Toshiba Launches 12-Watt Receiver IC for Fast Wireless Charging of Tablet Devices

 January 6, 2015

Extending capability to tablet devices intended to speed wireless power technology adoption


CONSUMER ELECTRONICS SHOW (CES), LAS VEGAS, — Toshiba America Electronic Components, Inc. (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today introduced its newest IC enabling wireless mobile device charging. The TC7765WBG wireless power receiver controller IC effectively manages the 12-watt power transfer necessary for wireless charging of tablet devices. Compatible with the Qi low-power specification version 1.1 defined by the Wireless Power Consortium (WPC), the new IC delivers a user experience comparable to that of conventional wired charging for tablets, as well as smartphones and other portable devices. TAEC will demonstrate the new receiver IC this week at CES 2015 in Las Vegas, Nevada.

ABI Research1 forecasts that the installed base of mobile devices - tablets, smartphones, wearables, notebooks and basic mobile phones - will reach 8 billion by 2019. This will, in turn, create a huge installed base for rechargeable batteries and charging solutions, including wireless solutions enabled by the Toshiba controller IC portfolio.

"While wireless power technology is growing in popularity, broader adoption has been hindered by the lack of a solution with sufficient power to wirelessly charge tablet devices," said Deepak Mithani, senior director of the Mixed Signal Business Unit, System LSI Group at TAEC. "With this addition to our portfolio of wireless charging ICs, Toshiba is taking an active role in driving the industry to clear this hurdle so that it can keep pace with consumer demand."

The TC7765WBG wireless power receiver controller IC is built with Toshiba's mixed-signal process using a high-performance MOSFET design that maximizes power efficiency and thermal performance. The IC combines modulation and control circuitry with a rectifier power pickup, I2C interface and circuit protection functions. Compliance with the "Foreign Object Detection" (FOD) aspect of the Qi specification prevents heating of any metal objects in the path of wireless power transfer between the receiver and the transmitter.

The 12W receiver IC is designed in the same size package as Toshiba's 5W wireless power receiver controller TC7763WBG - a compact WCSP-28 2.4mm x 3.67mm x 0.5mm package - further facilitating design-in and contributing to the new chipset's backward compatibility with the lower-power receiver IC. Combining the TC7765WBG with a copper coil, charging IC and peripheral components creates a wireless power receiver. Joining the receiver with a Qi-compliant wireless power transmitter containing a Toshiba wireless power transmitter IC (such as TB6865AFG Enhanced version) forms a complete wireless power charging solution.

Samples of the TC7765WBG wireless power receiver IC will be available at the end of this month, with mass production set to begin in Q2 2015.

*About TAEC

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today's leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's sixth largest semiconductor manufacturer (Gartner, 2013 Worldwide Semiconductor Revenue, April 2014). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 590 consolidated companies employing over 200,000 people worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.

1Findings are part of ABI Research's "Wearables and Smart Accessories Market Research," October 2014.


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice.
 

WRLS 15 736

A new window will open