Contact us

A new window will open A new window will open

Toshiba Licenses ARM Cortex-A53 High-performance Microprocessor

TOKYO—Toshiba Corporation (TOKYO: 6502), July, 30, 2015 -  today announced that it has licensed the ARM® Cortex®-A53 processor, the most power-efficient ARMv8-A processor capable of seamlessly supporting 32-bit and 64-bit code. Toshiba will deploy the processor to develop ASSPs (Application Specific Standard Products), such as ApP Lite™ application processors that offer well balanced power-efficiency and performance with 64-bit capability, and custom products such as FFSA™ (Fit Fast Structured Array) and ASIC(Application Specific Integrated Circuit) for industrial, networking, IoT, automotive and data storage products. The Company expects to bring products to market at an early date.
 

The industrial market is seeing strong demand for 64-bit capabilities and high reliability. The network market requires high-speed, low-power-consumption operation, real time processing and multi-clustered storage systems1 for handling huge volumes of data and data encryption. IoT products require power-efficient microprocessors, and applications relying on enormous storage capacity need an expanded memory address space. Toshiba will develop products to meet these various demands.
 

The processor will allow Toshiba to hasten the development of highly featured, high performance systems that meet the functional safety requirements of ISO26262 for the automotive market and to provide customers with solutions for next generation automotive applications.
 

The Cortex-A53 processor features an 8-stage in-order pipeline2, and strengthened data access / instruction fetch techniques. It also features ARM NEON™ technology with enhanced multimedia handling capabilities in addition to 128-bit SIMD ordering capabilities, as well as a cryptographic engine that accelerates encryption handling such as AES (Advanced Encryption Standard) and SHA (Secure Hash Algorithm) by extending architectures.
 

"Toshiba’s commitment to build SoCs based on Cortex-A53 further highlights the diverse range of use cases for the industry’s leading low-power 64-bit processor," said Nandan Nayampally, vice president, marketing, CPU group, ARM.  "The Cortex-A53 will deliver new levels of compute performance into power and space constrained environments in automotive, IoT and networking infrastructure applications and the processor safety package enables Toshiba to create products compliant with the latest functional safety standards."
 

Adding the Cortex-A53 processor to its ARM portfolio will allow Toshiba to strengthen its wide product line-up and improve product competitiveness. Toshiba will continue to enhance its semiconductor business by constantly introducing optimized ARM processor cores to meet a wide range of customer needs.


1 Multi-clustered storage systems: Systems with multiple processor architectures.
2 Pipeline: Divides instruction procedures into separate parts (stages), such as fetch, decode, execute and data commit, in order to perform multiple operations at the same time and to increase instruction throughput.

* ARM, Cortex and NEON are registered trademarks or trademarks of ARM Limited (or its subsidiaries) in the EU and/or elsewhere. FFSA and ApP Lite are trademarks of Toshiba Corporation. All other trademarks and trade names are properties of their respective owners.

Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.
 

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.