Contact us

A new window will open A new window will open

Toshiba Introduces N-Channel MOSFETs for Load Switching in USB Type-C Mobile Devices

Feature Industry-Leading Low On-Resistance

IRVINE, Calif., November 29, 2016 -- Toshiba America Electronic Components, Inc. (TAEC)* has expanded its lineup of small, low on-resistance MOSFETs with the addition of the SSM6K513NU and SSM6K514NU. The new N-channel MOSFETs feature industry-leading1 low on-resistance, and are suited for use as load switches in mobile devices such as smartphones and tablets.

The 30V SSM6K513NU and 40V SSM6K514NU utilize Toshiba’s latest U-MOS IX-H series trench process, which is designed to deliver efficiency across a wide range of load conditions by driving down on-resistance (RDS(ON)) and improving switching efficiency by reducing output charge (QOSS) 2. The SSM6K513NU and SSM6K514NU achieve on-resistance of 6.5mOhm and 8.9mOhm, respectively, and reduce heat dissipation resulting from turn-on loss by approximately 40 percent when compared to existing products. 3

The SSM6K513NU and SSM6K514NU can be used in electric power switching applications of over 10W, including small mobile devices that meet the USB Type-C™ and USB Power Delivery standards. Toshiba’s new MOSFETs contribute to high system efficiency and low power consumption in these space-conscious devices.

Main Specifications

Part Number

Absolute Maximum Ratings

RDS(ON) typ. (mOhm)

Ciss typ.






















Pricing and Availability

The SSM6K513NU and SSM6K514NU are available now. For more details, samples and pricing information, please contact your local Toshiba Sales Office.

*About TAEC

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide.  A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan’s largest semiconductor, solid state drive and hard disk drive manufacturer and the world’s seventh largest semiconductor manufacturer (Gartner, 2015 Worldwide Semiconductor Revenue, January, 2016). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 550 consolidated companies employing over 188,000 people worldwide (as of March 31, 2016). Visit Toshiba's web site at

1For products with the same ratings, as of September 26, 2016. Toshiba survey.
2Compared to existing products.
3Compared to Toshiba’s SSM6K504NU.

*USB Type-C is a trademark of the USB Implementers Forum.

Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.