Applications Include White LED Backlights, Liquid Crystal Displays
IRVINE, Calif., March 9, 2017 -- Toshiba America Electronic Components, Inc. (TAEC)* today announced that it has expanded its extensive portfolio of diodes with the addition of six low reverse-current Schottky barrier diodes (SBDs). With a peak reverse voltage of 40V, the new CCS15F40, CUS15F40, CBS10F40, CUS10F40, CTS05F40, and CUS05F40 are suitable for voltage boosting circuits in white LED backlights and for liquid crystal displays in mobile devices (including smartphones and tablet PCs).
The reverse current of the CCS15F40, one of the new products, is 25μA (max)1, and the new SBD’s thermal runaway temperature is 35°C higher than previous products, which contributes to stable circuit operations. The CCS15F40 features fast switching due to low total capacitance of 130pF (typ.) @VR=0V. A low reverse current contributes to the low power consumption of the device, making thermal runaways unlikely, even in high-temperature environments.
Toshiba's entire lineup of surface mounting diode products are available in many package types and sizes, making them suitable for today's applications where lightweight, compact size and high efficiency are of the utmost importance. In addition to the industry standard SOD-323 package, Toshiba has introduced leadless surface mounting packages (CST2C2, CST2B3) and SOD-882 packages (CST24) in to the SBD lineup, which contribute to making devices slimmer and smaller.
“As mobile devices become more and more sophisticated, the use of voltage boosting circuits of 30V or higher will increase,” noted Talayeh Saderi, senior business development manager for TAEC. “We will continue to add higher peak reverse voltage diodes to our product lineup to meet expected demand.”
Main Specifications
(@T a=25°C)
Part |
Absolute |
Forward voltage |
Forward voltage |
Reverse |
Package |
|||
---|---|---|---|---|---|---|---|---|
Reverse |
Average |
(V) |
@IF |
(V) |
@IF |
|||
40 |
1.5 |
0.35 |
0.1 |
0.64 |
1.5 |
25 |
CST2C |
|
1.0 |
0.38 |
0.1 |
0.70 |
1.0 |
20 |
CST2B |
||
0.5 |
0.45 |
0.1 |
0.81 |
0.5 |
15 |
SOD-882 (CST2) |
||
CUS15F40 |
1.5 |
0.35 |
0.1 |
0.65 |
1.5 |
25 |
SOD-323 (USC) |
|
1.0 |
0.38 |
0.1 |
0.67 |
1.0 |
20 |
SOD-323 (USC) |
||
0.5 |
0.45 |
0.1 |
0.81 |
0.5 |
15 |
SOD-323 (USC) |
Characteristic Curves
Pricing and Availability
The new SBDs are available now. For more details, samples and pricing information, please contact your local Toshiba Sales Office.
*About TAEC
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan’s largest semiconductor, solid state drive and hard disk drive manufacturer and the world’s seventh largest semiconductor manufacturer (Gartner, 2015 Worldwide Semiconductor Revenue, January, 2016). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 550 consolidated companies employing over 188,000 people worldwide (as of March 31, 2016). Visit Toshiba's web site at http://toshiba.semicon-storage.com.
1@VR=40 V
21.6×0.8 mm (typ.), t: 0.5 mm (max)
31.2×0.8 mm (typ.), t: 0.4 mm (max)
41.0×0.6 mm (typ.), t: 0.4 mm (max)
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.