Contact us

A new window will open A new window will open

Toshiba Introduces TR200 SATA Retail SSD Series with 64-Layer 3D Flash Memory

The all-new Toshiba TR200 Series delivers next generation upgrade for Mobile or Desktop Systems

IRVINE, Calif. — July 27, 2017 — Toshiba America Electronic Components, Inc. (TAEC), a committed technology leader, today unveiled the TR200 SATA solid state drive (SSD) series for the retail market. Leveraging Toshiba’s advanced 3-bit-per-cell TLC (triple-level cell) BiCS FLASH™, the TR200 series offers PC gamers and DIY enthusiasts Toshiba’s first upgrade SSD with 64-layer 3D flash memory. 


Toshiba TR200 SSDs are an easy and affordable way to enhance notebook or desktop experiences by increasing system responsiveness and productivity over traditional hard disk drives (HDDs).  With a 6Gbit/s SATA interface, the TR200 series is rated for sequential read/write speeds(1) of up to 550 MB/s and 525 MB/s(2) and random read/write performances(3) of up to 80,000 and 87,000 input/output operations per second (IOPS)(4). In addition to excellent SATA performance, TR200 SSDs provide low power consumption that translates into a longer battery life for on-the-go users.


“We are excited to provide consumers with the new TR200 series, our first retail branded SATA 6Gbit/s drives to leverage state-of-the-art Toshiba 64-layer TLC BiCS FLASH™,” said Alex Mei, vice president consumer SSDs and storage outbound marketing, at Toshiba America Electronics Corporation, Inc. “Seeking to provide enhanced real world performance and value to customers, the TR200 SSDs were engineered from the ground up utilizing the latest 3D flash memory technology to be a cost-effective and power-optimized storage solution for desktop and mobile upgraders, gamers, and system builders.”


The TR200 series will be showcased at the China Digital Entertainment Expo & Conference (ChinaJoy) in Shanghai, China from July 27-30 and GamesCom in Cologne, Germany from August 22-26. TR200 drives will be offered in a 2.5-inch form factor and are available in 240GB, 480GB, and 960GB capacities(5) and will be available at retailers and etailers this Fall.


For more information on Toshiba’s line of industry-leading SSDs, please visit: http://toshiba.semicon-storage.com/us/product/storage-products.html. To learn more about Toshiba’s storage solutions, follow @ToshibaStorage on Twitter.


About Toshiba Corp. and Toshiba America Electronic Components, Inc. (TAEC)

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.


Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan’s largest semiconductor, solid state drive and hard disk drive manufacturer and the world’s seventh largest semiconductor manufacturer (Gartner, 2015 Worldwide Semiconductor Revenue, January, 2016). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 550 consolidated companies employing over 188,000 people worldwide. Visit Toshiba's web site at http://toshiba.semicon-storage.com.


(1)Sequential performance is measured with Iometer 1.1.0
(2)TMC survey based on sequential read and write speeds of 128KiB units, using TR200 series models under TMC test conditions. Read and write speed may vary, depending on the host device, read and write conditions, and file size. TMC defines a megabyte (MB) as 1,000,000 bytes and a kibibyte (KiB) as 210 bytes, or 1,024 bytes.
(3)Random performance is measured with CrystalDiskMark 5.1.2
(4)TMC survey based on random read and write speeds of 4KiB units, using TR200 series models under TMC test conditions. Read and write speed may vary, depending on the host device, read and write conditions, and file size. TMC defines a kibibyte (KiB) as 210 bytes, or 1,024 bytes
(5)Definition of capacity: Toshiba Memory defines a megabyte (MB) as 1,000,000 bytes, a gigabyte (GB) as 1,000,000,000 bytes and a terabyte (TB) as 1,000,000,000,000 bytes. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1GB = 230 = 1,073,741,824 bytes and therefore shows less storage capacity. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system, such as Microsoft Operating System and/or pre-installed software applications, or media content. Actual formatted capacity may vary.

*Company names, product names, and service names mentioned herein may be trademarks of their respective companies.


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.