Contact us

A new window will open A new window will open

Toshiba Introduces New, Compact N-Channel Power MOSFETs for Load Switching in Industrial, Automotive and Lighting Applications

IRVINE, Calif., October 17, 2017 --- Toshiba America Electronic Components, Inc. (TAEC)* today announced the expansion of its lineup of automotive N-channel power MOSFETs with the addition of the 60V SSM3K341R and the 100V SSM3K361R. Housed in small SOT-23F packages, the new MOSFETs feature industry-leading1 low on-resistance and are suited to load switching in LED driver applications, including automotive dashboard meters and headlights and LED TV backlights. 


Increasing demand for power-saving LEDs has led to the growing use of N-channel MOSFETs as switches for LED drivers. Toshiba’s SSM3K341R and SSM3K361R address this demand with the industry’s best typical RDS(ON) ratings (@VGS=4.5V) of 36mΩ and 65mΩ, respectively. Additionally, both devices support a maximum channel temperature of 175°C, which enables them to be used in a wide range of industrial and automotive applications.


The SSM3K341R and SSM3K361R reduce heat dissipation resulting from turn-on loss by approximately 65 percent when compared to previous products2. The small package size of the new MOSFETs maintains the same level of heat dissipation while reducing the overall footprint by approximately 64 percent when compared to a conventional SOT-89 package. Both products are AEC-Q101 qualified for automotive applications.


Toshiba has also introduced four new MOSFETs with even smaller package sizes. The SSM6K341NU and SSM6K361NU utilize the SOT-1220 package; while the SSM3K341TU and SSM3K361TU are housed in UFM (2.0×2.1mm) packages. These MOSFETs feature the same low on-resistance as the SSM3K341R and SSM3K361R, while reducing the package mounting area by 43 percent and 40 percent, respectively.


Main Specifications
(@Ta=25°C)

Part Number

Absolute Maximum Ratings

RDS(ON) typ. (mΩ)

Ciss typ.

VDSS

VGSS

ID

VGS=4.0V

VGS=4.5V

VGS=10V

(pF)

(V)

(V)

(A)

SSM3K341R

SSM3K341NU

SSM3K341TU

60

±20

6

43

36

28

550

SSM3K361R

SSM3K361NU

SSM3K361TU

100

±20

3.5

-

65

51

430

Both devices have a maximum allowable power dissipation rating of PD=1W (DC), 2W (10s).
 

Pricing and Availability

The SSM3K341R, SSM6K341NU, SSM3K341TU, SSM3K361R, SSM6K361NU, and SSM3K361TU are available now. For more details, samples and pricing information, please contact your local Toshiba Sales Office.


*About Toshiba Corp. and Toshiba America Electronic Components, Inc. (TAEC)

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs and distributors. A committed electronic components leader, Toshiba designs and manufactures high-quality hard disk drives (HDDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, and advanced materials that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions, consumer products and more.


Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc. For over 140 years, Toshiba Corporation has contributed to a sustainable future by applying innovative technologies to value creation. Today, our business domains are centered on the essential infrastructure that supports modern life and society. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future”, Toshiba promotes global operations that contribute to realization of a world where generations to come can live better lives. Visit Toshiba's web site at http://toshiba.semicon-storage.com


1Products with the same ratings, as of June 23, 2016. Toshiba survey.
2Compared to Toshiba’s SSM3K318R


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.