Contact us

A new window will open A new window will open

Toshiba Announces 10TB NAS-Class Hard Drive

The MN06ACA10T Series provides 25 percent more capacity over prior generation models

IRVINE, Calif. — December 4, 2017 — Toshiba America Electronic Components, Inc., a committed technology leader, announces the MN06ACA10T, the latest addition to its MN Series lineup of 3.5-inch hard drives for use in NAS platforms. The new 10 TB1  model is designed to operate 24/7 to help organizations of all sizes manage data growth effectively. The newest MN06 Series is suitable for NAS filer and cloud storage applications that require disk drives with a workload rating of 180 TB per year2.


The MN06ACA10T features a maximum sustained transfer rate of 237 MiB/s3 and is designed for 300,000 load/unload cycle robustness. The drive provides a SATA 6 Gbit/s interface and 7,200 rpm access performance. The MN06ACA10T supports Advanced Format (512e) technology for compatibility with legacy applications and operating environments and are compatible with popular third party NAS appliances.


 “Our new 10 TB MN06 Series provides excellent NAS-class performance and durability,” said Scott Wright, Director of HDD Product Marketing at Toshiba America Electronic Components, Inc. “Our exclusive conventional mechanics delivers real value to work-groups and cloud storage architects who utilize established network-attached storage technologies. The MN06ACA10T 10 TB includes RV compensation technology for optimal performance in multi-drive NAS enclosures and is designed for 24/7 operation.”


Samples of the MN06ACA10T are now available. For more information on Toshiba HDD storage products, please visit: http://toshiba.semicon-storage.com/us/product/storage-products.html. To learn more about Toshiba storage solutions visit the storage blog at http://storage.toshiba.com/corporateblog/ and follow @ToshibaStorage on Twitter.


About Toshiba Group. and Toshiba America Electronic Components, Inc.

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba Group enables its customers to create market-leading designs. Toshiba Group is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs,  distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba Group designs and manufactures high-quality hard disk drives (HDDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, and advanced materials that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions, consumers and more.


Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc. For over 140 years, Toshiba Corporation and its affiliates/subsidiaries have contributed to a sustainable future by applying innovative technologies to value creation. Today, our business domains are centered on the essential infrastructure that supports modern life and society. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future”, Toshiba Group promotes global operations that contribute to realization of a world where generations to come can live better lives. Visit our web site at http://toshiba.semicon-storage.com.


1Definition of capacity: A terabyte (TB) is 1,000,000,000,000 bytes. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1TB = 240 = 1,099,511,627,776 bytes and therefore shows less storage capacity. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system and/or pre-installed software applications, or media content. Actual formatted capacity may vary.
2Workload is a measure of the data throughput of the year, and it is defined as the amount of data written, read or verified by commands from the host system.
3
A mebibyte (MiB) means 220, or 1,048,576 bytes. Read and write speed may vary depending on the host device, read and write conditions, and file size.

Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Company names, product names, and service names mentioned herein may be trademarks of their respective companies.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.