How can I calculate current and power consumption?

Broadly speaking, the power consumption of a motor driver consists of two factors: the power consumed due to the IC bias current and the power consumed due to current flowing through the output section. Both these factors are affected by the drive voltage and the duty cycle.
For details of how to calculate the power consumption of a motor driver, see the appropriate datasheet or contact us.

A new window will open