Contact us

A new window will open A new window will open

Partner Information

Listed in alphabetical order

  • A.I. Corporation

    A.I. Corporation, a solutions vendor, provides marketing, development and engineering services focused on the engineering of software for embedded systems, communications and networks.

    Product Introduction
    Category Product name MCU
    OS TOPPERS-Pro TX03 Series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • ADLINKS Corp.

    ADLINKS Corp. is an innovative company that specializes in sockets, adapters, harnesses and boards for high-speed transmission with the aim of ensuring "comfortable user interface". The ADLINKS products supporting Toshiba's development systems include the probe sets for the TLCS-870/C and TLCS-870/C1 emulators, MCU mounting adapters (Bump Sockets) and simple EV boards.

    Product Introduction
    Category Product name MCU
    Socket, Connector Bump socket
    Probe set
    Test clip
    TLCS-870/C Series
    TLCS-870/C1 Series
    Board/Evaluation kit Simple evaluation board
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • Andor System Support Co., Ltd.

    Andor System Support Co., Ltd. is one of the training centers certified by ARM Ltd. in UK. Our seminars of TX03 and TX09 series are so effective for engineers who develop the systems or consider using them.
    And as an embedded system integrator we accept customized development of either hardware or software design using TX03 and TX09 series. Our rich experiences and great performance support you at every development stage such as system design, integration, and maintenance.
    Our boundary scan test system is a tool to do test and on-board programming which needs only 5 signal pins. It is one of the best solutions to test high-density print-circuit boards on which BGA-package devices, etc are mounted. It achieves the test and on-board programming at all stages including sample development stage and mass production one.

    Product Introduction
    Category Product name MCU
    Boundary Scan Test
    FLASH programmer/Writer
    JTAG ProVision
    ProVision Designer station
    JTAG Live
    TX03 and TX09 series with function of Boundary Scan Test
    Business Information
    Category Detailed information MCU
    Teaching Materials/Seminar Cortex™–M3 Software Design Course certified by ARM (3 days) TX03 series
    TX09 series
    Software development/SI Customized development of software and hardware TX03 series
    TX09 series
    FLASH programming service TX03 series
    TX09 series

    Boundary Scan Test System by JTAG Technologies

    JTAG ProVision

    This tool can detect instantly failure portions of solder errors and pattern errors. The machine cost is in the lowest level because only 5 pins are necessary for the test. The test codes are generated automatically by following its wizards, so preparation for the test can be completed while the target board is under production.

     

    JTAG ProVision

     

    JTAG ProVision components
    JTAG ProVision This tool generates test codes from a circuit net list and information in BSDL file, and executes the test.
    Boundary Scan Controller This is a hardware which tests a target board and does on-board programming.
    Failure Analysis Software / Visualizer This tool identifies an error status such as open, short-circuits, etc. for the failure pins or the failure nets, and also highlights the failure portions on the circuit diagram and the board layout.
    On-board Programming for Flash Memory and cPLD This tool generates automatically control programs to write Flash memories (also available for embedded Flash Memories) and cPLDs.
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

     For detailed information, visit the website of Andor System Support Co., Ltd.

  • ARM Ltd. (KEIL)

    Keil MDK-ARM™ is a complete software development environment for Cortex™-M, ARM7™ and ARM9™ processor-based devices.MDK-ARM, which is specifically optimized for microcontroller applications, contains the ARM C/C++ Compiler, the μVision IDE and Debugger, the Keil RTX real-time operating system and middleware libraries. ARM DS-5™ (Development Studio 5) is a software development tool suite for ARM processor-based ASICs and standard devices. ARM provides versatile, high-performance and easy-to-use development environments for software developers.

    Product Introduction
    Category Product name MCU
    IDE/Compiler RealView® MDK
    µVisiion®
    TX00 Series
    TX03 Series
    TX04 Series
    Debugger U-LINK2®
    U-LINK® PRO
    Board/Evaluation kit MCBTMPM330UME [TMPM330]
    MCBTMPM362UME [TMPM361/TMPM362]
    MCBTMPM364UME [TMPM363/TMPM364]
    MCBTMPM365UME [TMPM365]
    MCBTMPM369UME [TMPM367/TMPM368/TMPM369]
    MCBTMPM395UME [TMPM390/TMPM395]
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

    Starter Kit for Toshiba ARM Core-based Microcontrollers

    MCBTMPM330UME

    Users can start with this kit for evaluating their system. From the code generation phase, users can write to the Flash memory to execute them.

    Starter Kit for Toshiba ARM Core-based Microcontrollers 

     

    Product configuration of MCBTMPM330UME
    MCBTMPM330 evaluation board An evaluation board featuring a Toshiba TMPM330FDFG.
    It offers three LEDs, 1-bit switch input, NMI (Non-Maskable Interrupt), a reset switch, a potentiometer to test AD conversions. 10-MHz clocker supply to the microcontroller which is used as 40-MHz operation clock. A new 0.05-inch-pitch connector for future use of instruction trace. Powered from USB, no external power supply is required. Pin access to external circuits.
    ULINK-ME USB-interface ICE USB-interface ICE gives easy connection with PC.
    Evaluation version MDK IDE (Integrated Development Environment) Since Serial-Wire debug is supported, data can also be read out in real time.
    Blinky demonstration A demonstration that changes a period of time blinks the LED according to angles of the potentiometer. Users can build program and write to a flash memory, with/without the ICE. Using this demonstration, users can learn header files provided by RealView MDK, interrupt processing, and how to write program for TMPM330.

     For detailed information, visit the website of ARM, KEIL product team of Sohwa & Sophia Technologies Inc. or Yokogawa Digital Computer Corporation.

  • Atollic AB

    The Atollic TrueSTUDIO® is an embedded system tool that will meet your needs for the next 10 years. Built on the ECLIPSE IDE framework, TrueSTUDIO® can be seamlessly integrated with existing embedded systems, improving development productivity and user-friendliness. TrueSTUDIO® provides C/C++, build/debug and simulation to ols for t he Toshi ba TX processors and enables algorithm testing even before a hardware interface is available. Additionally, it supports features that facilitate team collaboration such as migration paths from UML models to software solutions, a version management system and a bug/task database system.

    Product Introduction
    Category Product name MCU
    IDE/Compiler TrueSTUDIO/TX TX00 Series
    TX03 Series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • BITRAN CORPORATION

    JeRana is a JTAG emulator that supports the TX03 Series. Designed specifically for Cortex™-M3, JeRana is priced lower than its predecessors. Above all, JeRana is small and easy to use. To improve your productivity, JeRana provides basic debugging features and is capable of directly programming Flash ROM integrated in MCUs.

    Product Introduction
    Category Product name MCU
    Debugger JeRana TX03 Series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • CATS CO.,LTD.

    ZIPC from CATS is a CASE tool based on a state transition matrix targeting embedded applications. Use of a state transition matrix for design and simulation helps prevent specification oversights. ZIPC provides an automatic code generation capability; it allows you to generate MISRA-C-compliant reliable source code from a state transition matrix that represents your design requirements. Additionally, using ZIPC in tandem with the Toshiba Integrated Development Environment, TIDE, allows target debugging while viewing the state transition matrix. This greatly improves development productivity and quality.

    Product Introduction
    Category Product name MCU
    Simulator
    Upstream design tool
    ZIPC TX19A/H Series
    TX19A Series
    TLCS-900 Family
    TLCS-870/C1 Series
    TLCS-870/C Series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • Computex Co.,Ltd.

    Computex manufactures development support systems that assist in debugging embedded software. A seamless development environment is available for the TX03 Series that encompasses everything from evaluation and development to the production phase. The PALMiCE3 JTAG emulators support various target interfaces such as JTAG and ETM. The on-chip flash programmer, FP-10, provides a standalone mode that does not require a host PC and operates at 3 to 5 V. ROMiCEmini supports the TX19A and TLCS-900/H1 Series.

    Product Introduction
    Category Product name MCU
    IDE/Compiler ARM Compiler for Computex TX00 Series
    TX03 Series
    TX04 Series
    Debugger PALMiCE3
    FLASH programmer/Writer FP-10
    Board/Evaluation kit M362F10 EVA BOD
    MiddleLink, CM-J series
    Debugger ROMiCE mini TMP19A31C
    TLCS-900/H1 Series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • CooCox

    CooCox, from element14 Embest, provides a complete set of FREE software tools enabling rapid development and debugging of full-featured applications for ARM Cortex-M based devices. These tools include the CoIDE, an Eclipse and GCC based IDE (Integrated Development Environment) with enhancements and simplification specific to Cortex M development, enabling embedded developers using TX03 series to develop applications from initial evaluation through to final production. In particular, with the integrated code component platform for uploading and downloading reusable code components, CoIDE can organize, extract, and share expertise through the collective wisdom.

    Product Introduction
    Category Product name MCU
    IDE/Compiler CoIDE TX00 series
    TX03 series
    Debugger CoLink,CoLinkEX
    FLASH programmer/Writer CoFlash
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • eForce Co., Ltd.

    eForce offers μC3/Compact, a μTRON-compliant compact RTOS, μNET3/Compact, a TCP/IP protocol stack that operates only with a CPU's internal memory, etc. eForce supports ARM Cortex™-M and other ARM core-based microcontrollers to address customer needs to reduce development time and win a valuable time-to-market edge. It offers μC3/Compact for the TX03 Series and μC3/Standard for the TX09 Series.

    Product Introduction
    Category Product name MCU
    OS µC3/Compact TX03 series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • Elnec s.r.o.

    Elnec develops and manufactures universal programmers for engineering and volume production. The company offers high quality and well designed products at very affordable level of prices. Majority of Elnec device programmers includes a 3 years warranty. Updates of programmer's software are released according to the customers’ needs (in many cases daily) and download of the new software version is available free of charge. For more information please visit Elnec's website. Elnec supports an extensive range of Toshiba programmable devices and support grows with each version of new programmer's software.

    Product Introduction
    Category Product name MCU
    FLASH programmer/Writer BeeProg2 series
    (BeeHive208S, BeeHive204)
    TX03 Series
    TLCS-900/L1 Series
    TLCS-870/C1 Series
    TLCS-870/X Series
    TLCS-870/C Series
    TLCS-47 Family
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • ESP Co., Ltd.

    With all our technical capabilities and corresponding speed, we serve customers from circuit design of embedded system, art work, board manufacture, part procurement, mounting, examination to software development. We can support customers to develop ARM® Cortex™-M Core-based products using our experiences of developing a number of evaluation boards.
    Through being involved in publishing ‘Vector Control Technology for Brushless DC Motors’ (CQ Publishing Co., Ltd.), we can deliver lectures on TMPM370 series with Vector Engine in any parts of the nation.


    Product Introduction

    1. Development of industrial system
    2. Supports from circuit design, board development, part procurement, alignment, mounting, examination to software development.
    3. Development of embedded software.
    4. Development, production and distribution of platform boards for microcontroller development.
    5. Development, production and distribution of microprocessor applied equipment.
    6 .Development, production and distribution of digital educational materials and educational robots.

  • Falcon Denshi K.K.

    Falcon Denshi is a subsidiary of Hi-Lo Systems in Japan. It offers device programmers and automated programming systems worldwide under the brand names of Hi-Lo Systems and FALCON. It also offers device programming services using its facilities in Japan, Taiwan, Hong Kong, China, Singapore, etc. Falcon Denshi supports the ARM core-based TX03 Series, TLCS-900/H1Series, TLCS-47E Series, TLCS-870/C1 Series and so on. Its product portfolio includes ALL-100AX, a single-device programmer for engineering, gang programmers that allow simultaneous programming of 4 to 8 devices for medium-scale production, and automated programming systems that support programming of 900 to 2200 devices per hour. Falcon Denshi also offers custom algorithm development services.

    Product Introduction
    Category Product name MCU
    FLASH programmer/Writer ALL-100AX TX00 Series
    TX03 Series
    TX19 Series
    TLCS-900 Family
    TLCS-870 Family
    TLCS-47 Family
    Business Information
    Category MCU
    FLASH programming service TX00 Series
    TX03 Series
    TX19 Series
    TLCS-900 Family
    TLCS-870 Family
    TLCS-47 Family
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • GAIA System Solutions Inc.

    GAIA System Solutions Inc. is engaged in the sales of high-speed software/hardware co-simulators for embedded software development and related support and consulting services. Supported CPU models include the TX19 Series, TX19A Series and TX19A/H1 Series. Toshiba Integrated Development Environment (TIDE) and MULTI® from Green Hills Software, Inc. support debugging environment without changing the customer's current development environment.

    Product Introduction
    Category Product name MCU
    Simulator CoMET. METeor TX19A/H1 Series
    TX19A Series
    TLCS-870/C Series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • GAIO TECHNOLOGY CO.,LTD.

    GAIO TECHNOLOGY develops and offers tools for improving the quality of embedded software, such as CoverageMaster winAMS, a unit testing tool for embedded software, No. 1 System Simulator that uses a high-speed MPU simulator, and CasePlayer2, a program chart and specification document generation tool. These tools support the latest ARM-based TX03 Series in addition to TX19, TLCS-900 and TLCS-870.

    Product Introduction
    Category Product name MCU
    Simulator Coverage master TX03 Series
    TX04R Series
    TX19A/H1 Series
    TLCS-870/C Series
    TLCS-900/L Series
    TLCS-900/H Series
    IDE/Compiler Case Player2 All Family
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • GRAPE SYSTEMS INC.

    Grape Systems offers the GR-USB USB stack series for the TX03 Series, various class drivers such as a Mass Storage Class driver, the GR-FILE FAT system, the ThreadX high-speed real-time operating system, the NetX networking protocol, etc. Grape Systems also provides custom development services. Contact Grape Systems for details.

    Product Introduction
    Category Product name MCU
    OS GR-USB Series
    ThreadX, ThreadX-µITRON
    TX03 Series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • Green Hills Software/Advanced Data Controls Corp.

    Advanced Data Controls Corporation (ADaC) has been a partner of Green Hills Software,Inc. (GHS) for 20 years in sales and technical support in Japan and other Asian countries. GHS offers total solution support for compilers, debuggers and JTAG probes to help you create applications for Toshiba's ARM Cortex core-based microcontrollers. It delivers overwhelming compiler performance in terms of speed and code size.
    (Please refer to the 28-Mar-2012 article in "News Releases" in GHS website.)

    GHS MULTI Tool Chain has received the highest level of certification ISO 26262 ASIL D for tool qualification requirements from TÜV Nord on September 2012.
    (Please refer to the 18-Sep-2012 article in "News Releases" in GHS website.)

    ADaC and GHS provide technical support to help you improve your application performance.

    Product Introduction
    Category Product name MCU
    IDE/Compiler MULTI
    * Made by GHS company
    TX03 Series (TMPM350 Group)
    TX04R Series (TMPR450 Group)
    TX19A Series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • HI-LO SYSTEMS RESEARCH CO.,LTD

    ALL-100A programmer from HI-LO SYSTEMS has 68 sets of Precise Universal Pin Driver to provide high speed, low noise, accurate and reliable programming signals for various IC products including high speed low power devices recently released to market.
    ALL-100A can be setup for either single-site programming for engineering or multi-site programming for production. If required, up to 8 sets of ALL-100A can be setup for multi-set operation so up to 64 sites can be programmed simultaneously to maximize production.
    Supporting software for ARM core-based TX03 Series, TLCS-900/H1 Series, TLCS-47E Series and TLCS-870/C1 Series etc. are available now. Device support on web site for check / retrieve through Internet will be updated on weekly basis.

    Product Introduction
    Category Product name MCU
    FLASH programmer/Writer ALL-100AX TX00 Series
    TX03 Series
    TX19 Series
    TLCS-900 Family
    TLCS-870 Family
    TLCS-47 Family
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • IAR Systems AB

    IAR Systems offers development environment for ARM core-based TX00/03/03/09 Series.
    Especially for TX03 Series a variety of inexpensive evaluation kits are available. The IAR evaluation kit consists of a target board, an integrated development environment (evaluation version), a JTAG in-circuit emulator and ready-to-run sample application programs. You can readily use it for the entire development cycle from device evaluation to application-level prototyping and evaluation. You can save significant time and costs otherwise needed at the onset of development. The evaluation kits of TX00 and TX04 Series will be released soon.

    Product Introduction
    Category Product name MCU
    IDE/Compiler EWARM (IAR Embedded Workbench for ARM) TX00 Series
    TX03 Series
    TX04 Series
    TX09 Series
    Debugger I-jet、JTAGjet、JTAG-Trace
    Board/Evaluation kit KSK-TMPM061        [TMPM061]
    KSK-TMPM330-TPL [TMPM330]
    KSK-TMPM341        [TMPM341]
    KSK-TMPM364-JL   [TMPM363/TMPM364]
    KSK-TMPM365-JL   [TMPM365]
    KSK-TMPM366        [TMPM366]
    KSK-TMPM369        [TMPM367/TMPM368/TMPM369]
    KSK-TMPM370-TPL [TMPM370]
    KSK-TMPM376-TPL [TMPM376]
    KSK-TMPM380-TPL [TMPM380]

    IAR Systems AB Starter Kit for Toshiba ARM Core-based Microcontrollers (one sample)

    KSK-TMPM369

    This evaluation board for the TMPM369FDFG incorporates the integrated development environment in Japanese language (evaluation version) and the JTAG-ICE function. This “all in one” starter kit and attached sample application software support you to get started easily.

     

    KSK-TMPM369

     

    Product configuration of KSK-TMPM369
    JTAG emulator JTAG/SWD-ICE (on board)
    Evaluation board TMPM369FDFG ARM 32 bit Cortex-M3 microcontroller
    JTAG connector (ARM compatible/not included),
    On-board debugger (control through USB),
    Trace connector (not included), 4 ways power supply:
    USB, JTAG, Power supply jacks, On-board debugger USB,
    Ethernet connector,
    USB driver and connector/ Host connector, Device connector, RS232 driver, UART connecter X 2, CAN connector, SD card slot, Reset button, Power indicator LED, User LED X 8, Joystick
    Size: 165 x 130 mm
    RoHS compliant
    Evaluation version compiler EWARM (IAR Embedded Workbench for ARM)
    Evaluation version RTOS μC/OS-II (by Micrium)
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

     For detailed information, visit the website of IAR Systems AB

  • KibanHonpo(Japan Circuit)

    At KibanHonpo, We are now selling various kind of Microcomputer Module and Evaluation Boards . Peripherals needed to develop the base board of microcomputer modules are also available in various stocks. We offer original evaluation boards at reasonable price.

    Product Introduction
    Category Product name MCU
    Board/Evaluation Kit TMPM36BFYFG/F10FG
    Evaluation Board
    TX03 Series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • KYOCERA Corporation

    KYOCERA Corporation produces a wide variety of electronic components which answer the needs of the age. The components’ high performances are achieved by KYOCERA with both high developing technology of various materials and sophisticated material-processing technology. KYOCERA has provided internet sites where customers can easily select the most preferable one from among a variety of its timing devices (Crystal units, kHz range crystal units, and Ceramic resonators) and also can find circuit constant values for the oscillator. And KYOCERA supplies test works to verify oscillation-matching to an LSI on demand from a customer at no charge.

    Product Introduction
    Category Product name MCU
    Electronic component Capacitors
    Crystal units
    kHz range crystal units
    Ceramic resonators
    TX03 Series
    TX09 Series
    TX19 Series
    TLCS-900 Family
    TLCS-870 Family
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • KYOEI co.,LTD.

    Kyoei designs and develops measurement control systems and Flash memory programming systems. Kyoei offers an on-board Flash programmer called I.S.P-310, which supports various Flash microcontrollers such as the Toshiba TX03 ARM core-based microcontroller series. The I.S.P-310 is small and lightweight and powered by two AA batteries. It is a standalone system and easily portable. You can use it in production lines and in the field.

    Product Introduction
    Category Product name MCU
    FLASH programmer/Writer I.S.P-310 TX03 series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • Kyoto Microcomputer Co.,Ltd.

    As a company specializing in debugger software and in-circuit emulators, Kyoto Microcomputer Co., Ltd. has been engaged in the improvement of embedded development environments. Its JTAG ICE, "PARTNER-Jet", offers a powerful and efficient debug environment to TX03 series and TX09 series, which incorporates advanced features ahead of other companies, for not only iTRON, but also operating systems with an MMU (Linux, Windows CE, T-Engine, etc.) that are recently adopted in high-end embedded environments, and also supporting multi-core processors.

    Product Introduction
    Category Product name MCU
    IDE/Compiler exeGCC TX03 Series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • Lauterbach Japan Ltd.

    We are a leading company specialized in on-chip debugger and trace tools for embedded program development.
    We provide versatile, investment-effective development environment. Modularization of each element enables users to share the common main body, which makes it possible to use various CPUs and MPUs. We can offer users very competitive price on the μTrace which can perform a trace analysis and advanced debugging for the devices of the Cortex™-M core series.

    Product Introduction
    Category Product name MCU
    Debugger TRACE32 ICD TX00 series
    TX03 series
    TX04 series
    TX09 series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • MICROTEK Inc.

    MICROTEK Inc. embarked on contract IC programming in 2000. Since then, the company has been building a successful track record in a wide range of fields including communications, information home appliances and automotive applications as a reliable provider of IC programming services.

    Business Information
    Category
    FLASH programming service
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • MINATO ELECTRONICS INC.

    MINATO ELECTRONICS INC. developed the first "device programmer" in Japan when PROM first came on the market. Since then, the company has been occupying the leading position in the programmer field. Its product line includes not only programmers but also auto programming equipment and exchange adapters for a wide variety of packages to meet various programming needs of customers. MINATO's programmers support the ARM-based TX03 series, as well as the TX19, TLCS-900, and TLCS-870 Families. Programming services using these products are also available.

    Product Introduction
    Category Product name MCU
    FLASH programmer/Writer Device programmer
    GANG programmer
    Toshiba's Flash microcontrollers
    Business Information
    Category MCU
    FLASH programming service Toshiba's Flash microcontrollers
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.


    The programming solution by a device programmer
     
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

      For detailed information, visit MINATO ELECTRONICS INC.

  • SEGGER Microcontroller GmbH & Co. KG

    SEGGER Microcontroller develops and distributes hardware and software development tools as well as software components for embedded systems designed with TX00/03/04/09 Series ARM MCUs.
    With ample experience in programming efficiently on embedded systems, SEGGER created highly integrated, cost-effective programming and development tools, such as the FLASHER (stand-alone flash programmer) and the industry leading J-Link / J-Trace debug probe. J-Link debug probe provides high download-speed into RAM and flash memory, and the ability to set an unlimited number of breakpoints in internal/external flash memory of MCUs.
    All software components (RTOS and Middleware) are feature-rich and high-performance with a very small footprint and outstanding documentation.
    SEGGER’s intention is to cut software development time for embedded applications by offering affordable, high quality, flexible and easy-to-use tools and software components allowing developers to focus more on their applications.

    Product Introduction
    Category Product name MCU
    Debugger J-Link PRO
    J-Link ULTRA+
    J-Link PLUS
    J-Link
    J-Trace Cortex-M
    J-Trace ARM
    TX00 Series
    TX03 Series
    TX04 Series
    TX09 Series
    FLASH programmer / Writer Flasher ARM
    Flasher Portable
    RTOS embOS (Real Time Operating System)
    Middleware embOS/IP (TCP/IP Stack)
    emWin (Graphic Software & GUI)
    emFile (File System)
    emUSB Device (USB Device Stack)
    emUSB Host (USB Host Stack)
    TX03 Series
    TX04 Series
    TX09 Series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • Sohwa & Sophia Technologies Co.,Ltd.

    Sohwa & Sophia Technologies offers embedded development solutions for Toshiba microcontrollers, such as Flash writers, emulators for the TX03 Series (ARM core-based microcontrollers), etc. Sohwa & Sophia Technologies has a proven track record in the design and development of custom boards and systems using Toshiba's microcontrollers. Being an authorized distributor of the ARM products (KEIL and DS-5), Sohwa & Sophia Technologies can provide a comprehensive solution, including an integrated development environment and a compile environment.

    Product Introduction
    Category Product name MCU
    FLASH programmer/Writer EJSCATT Writer
    EJ-Writer for TX19A
    EJ-Writer for TLCS Series
    TX00 Series
    TX03 Series
    TX04 Series
    TLCS-870 Family
    TLCS-900 Family
    TX19A/H1 Series
    TX19A Series
    Board/Evaluation kit TX19A23 Starter kit TX19A Series
    Debugger EJSCATT for ARM Cortex-M3 TX00 Series
    TX03 Series
    TX04 Series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • Techno Mathematical Co.,Ltd.

    Techno Mathematical Co.,Ltd. (TMC) develops and licenses image, audio, and voice related software IPs to realize high-quality sound and image, low CPU load an low power consumption.
    Our software IPs optimized for ARM core-based microcontrollers such as ARM CortexTM-series contribute to create customer’s superior products.

    Product introduction
    Categories Product names Relevant microcontrollers
    Middleware MP3 Encoder/Decoder
    AAC-LC Encoder/Decoder
    TX03 series
    TX04 series
    TX09 series
    H.264 BP Decoder TX09 series
    All product names mentioned are trademarks or registered trademarks of the respective companies.

  • Technohands Co., Ltd.

    Technohands Co., Ltd. is a company who provides a customer with a total solution including development, design, and production of motor driver systems. With using ultrasonic motors as well as conventional induction motors, our solution offers higher performance than current actuator systems which are applied to not only consumer products such as cell phones, digital cameras, and so on, but also FA machine utility.

    Product Introduction
    Category Product name MCU
    Electronic component Ultrasonic actuator, Linear actuator,
    Stepping motor, Voice coil motor
    TX03 Series
    * All brand names and product names are trademarks or registered trademarks of their respective companies. Information contained herein might be changed or updated without notice.

  • TOA ELECTRONICS, Inc. Flash Support Group Company

    TOA ELECTRONICS, Inc. Flash Support Group Company offers various semiconductor device tools mainly for Flash microcontrollers. The company’s product portfolio includes auto programming systems, a wide variety of programmers (covering low-cost on-board programming to development and mass-production programming) and peripheral tools. The programmers support an extensive range of devices including Toshiba’s TX19, TLCS-900 and TLCS-870 Families. Speedy and flexible programming services are also available.

    Product Introduction
    Category Product name MCU
    FLASH programmer/Writer On-board programmer
    Device programmer
    GANG programmer
    TX03 Series
    TX19A/H1 Series
    TLCS-900/H1 Series
    TLCS-900/L1 Series
    TLCS-870/C1 Series
    TLCS-870/C Series
    Business Information
    Category MCU
    FLASH programming service TX03 Series
    TX19A/H1 Series
    TLCS-900/H1 Series
    TLCS-900/L1 Series
    TLCS-870/C1 Series
    TLCS-870/C Series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • TOA ELECTRONICS, Inc. Hamatoh Company

    TOA ELECTRONICS, Inc. Hamatoh Company is an authorized distributor of Toshiba's microcontroller support products. In addition to the sales of various electronic components, TOA ELECTRONICS, Inc. Hamatoh Company is also engaged in the commercialization and online sales of boards and starter kits using Toshiba's microcontrollers. The company can deliver total services encompassing the designing, prototyping, volume production and inspection for MCU control circuitry, logic circuitry and analog circuitry with short delivery times.

    Product Introduction
    Category Product name MCU
    Board/Evaluation kit MCU board
    Starter kit
    TLCS-900/L1 Series
    TLCS-870/C1 Series
    TLCS-870/C Series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • Tokyo Eletech Corporation

    TOKYO ELETECH CORPORATION, a manufacturer of useful debug support tools, provides interface products for connecting Toshiba's emulators with microcomputer boards developed by customers. The company's main products include IC sockets for QFP, SOP and BGA, emulator connectors, exchange adapters, signal check boards and extension cables. TOKYO ELETEC also accepts custom orders in small quantities, utilizing the company's expertise in flexible/printed circuit board manufacturing techniques including fine cutting.

    Product Introduction
    Category Product name MCU
    Socket, Connector Probe set
    QFP adapter
    Pin protector
    TLCS-900 Family
    TLCS-870/X Series
    TLCS-870/C Series
    TLCS-870 Series
    TLCS-47 Family
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • TOSHIBA INFORMATION SYSTEMES (JAPAN) CORPORATION

    Toshiba Information Systems develops, sells and offers support services for μITRON4.0-compliant real-time operating systems (RTOS). It offers standard UDEOS4/Cortex™-M3 (compliant with μITRON4.0) for the TX03 Series that operates with on-chip ROM/RAM and UDEOS4/ARM (compliant with μITRON4.0), an enhanced version, for the TX09 Series. Also included among its product offerings is the compact UDEOS4/Lite for Cortex™-M0 and Cortex™-M3.

    Product Introduction
    Category Product name MCU
    OS UDEOS4/Cortex-M3 TX03 series
    UDEOS4/ARM TX09 series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • Toshiba Microelectronics Corporation

    We can deliver a complete testing solution to meet your requirements, such as consultation regarding LSI tests, test program creation, LSI failure analysis and circuit modification. For detailed information, refer to the website of the SoC Test & Analysis Services, Toshiba Microelectronics Corporation.

    Product Introduction
    Category
    SoC test, Analysis service
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • TOSHIBA PERSONAL COMPUTER SYSTEM CORPORATION

    Design, development and evaluation of embedded system products.

    We are making effort to develop products to meet customer’s requirements.
    We can develop related to system products of the Toshiba microcontrollers shown below using our experiences of commercialization of Toshiba’s microcontroller development tools.


    • Business Information
    Category Target microcontrollers
    Software development/SI TX00 series
    TX03 series
    TX04 series
    TX19 family
    TLCS-870 family

    The main services of Toshiba personal computer system are microcontroller development board designing and product technology and we have been developing many embedded systems and products. We also run development tool support websites and the help desk related to Toshiba microcontrollers.
    We can leverage our extensive experience and knowledge about Toshiba microcontroller, so we can provide consistent services ranging from product consulting, designing, development, manufacturing to maintenance services in order to support customers to develop embedded microcontroller boards and system products.

  • Ubiquitous Computing Technology Corporation

    UC Technology offers the source code of μT-Kernel, a tuned-up version of the latest μT-Kernel RTOS being standardized by the T-Engine Forum, as well as various sample programs. Since μT-Kernel comes with a project file for the integrated development environment, you can start creating μT-Kernel drivers and application software right after you have installed software without performing any complicated setup.
    You can purchase a royalty-free project license for μT-Kernel for mass production at a reasonable price.

    Product Introduction
    Category Product name MCU
    OS UCT µT-Kernel DevKit tuned Series TX03 Series
    TX04 Series
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • VAMOS

    With over 25 years of experience in EPROM programming, VaMos has been engaged in programming on-chip EPROM of Toshiba microcontrollers ever since its establishment in 1985. VaMos has been highly acclaimed by many customers for quick-turnaround, low-cost and high-quality services.
    Its mottoes are “Readiness,” “Quick Turnaround,” and “From Small Engineering Lots to Production Lots.” VaMos offers various adapters for Toshiba's OTP microcontrollers, Flash microcontrollers and ARM core-based microcontrollers. Contact VaMos if you need EPROM or Flash programming service.

    Business Information
    Category
    FLASH programming service
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • Yokogawa Digital Computer Corporation

    Yokogawa Digital Computer specializes in embedded solutions and offers an extensive range of products related to the design and development of microcomputer and peripheral systems. Included among its products are the “advice” series of in-circuit emulators, the NETIMPRESS series of flash microcontroller programmers, Windows Embedded CE starter kits and development process improvement tools. Yokogawa provides the ideal development environment by leveraging its experience and expertise. Yokogawa Digital Computer is an authorized distributor of and a certified training center for the ARM KEIL and DS-5. Thus, it can offer optimal solutions that best suit your need.

    Product Introduction
    Category Product name MCU
    IDE/Compiler microVIEW-PLUS TX03 Series
    TX49 Family
    TLCS-900/H1 Series
    ARM TX-03 Series
    Debugger advice series TX03 Series
    TLCS-900/H1 Series
    FLASH programmer/Writer MegaNETIMPRESS
    C"ar NET IMPRESS
    TX03 Series
    TX19 Series
    TX19A Series
    TX19A/H1 Series
    TLCS-900/H1 Series
    TLCS-900/L1 Series
    TLCS-900/H Series
    TLCS-870/C1 Series
    TLCS-870/C Series
    Business Information
    Category Detailed information
    Teaching Materials/Seminar Cortex™–M3 Software Design Course certified by ARM (3 days)
    *All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

  • ZLG (GUANGZHOU ZHIYUAN ELECTRONICS CO., LTD)

    Guangzhou Zhiyuan Electronics founded in May 2001 is engaged in design, production, and sales. It is a member of Field-bus DeviceNet ODVA China. The company has departments dedicated to development in specific fields, including the Industrial Communication Network Department, the Building Automation Department, the Measuring Instrument Technology Department, the Embedded System Application Department, the Power Supply Department, the OEM/ODM Product Department, the Computer Software Development Center, and the Industrial Design Center. The Measuring Technology Department focuses on the design and development of measuring and testing instruments and related development tools. It currently offers over ten types of products, including digital oscilloscopes, logic analyzers, protocol analyzers, digital multimeters, signal generators, universal emulators, and data collection cards. The products are widely applied in electronics design, manufacturing, industrial control, network communication, and scientific research. In accordance with its business philosophy, Guangzhou Zhiyuan Electronics emphasizes a faithful, customer-oriented approach.
    Proud of its tradition of high quality and excellent service, the company is ready to serve every customer in a spirit of wholehearted cooperation.

    Product Introduction
    Category Product name MCU
    IDE/Compiler TKStudio(GCC) TX03 Series
    Simulator Tkscope emulators
    FLASH programmer/Writer TKScope + K-Flash(On-board programming)
    SmartPRO programmers(Off-board programming)
    * All brand names and product names are trademark or registered trademark of their respective companies. Information contained herein might be changed or updated without notice.

Contacts

If you have any queries, click one of these links:

Technical queries
Queries about purchasing, sampling and IC reliability
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.