Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Keyword Search

Parametric Search

Stock Check & Purchase

Toshiba announces new cutting-edge CMOS silicon on insulator process

27th February 2020

New process will enhance the noise figure of RF switches and low noise amplifiers for 5G and Wi-Fi applications

Toshiba Electronics Europe GmbH has improved the characteristics of their silicon on insulator (SOI) process technology for RF switch /LNA ICs. The process, known as TaRFSOI™ (Toshiba RF SOI) is SOI-CMOS (silicon on insulator complementary metal oxide semiconductor), is an original front-end process technology that Toshiba developed for RF switch ICs.

As the performance of mobile devices including smartphones is constantly improving, their wireless frequencies are becoming higher. There are general concerns that receiving sensitivity deteriorates at higher frequencies in the same manner as signal loss increases between an antenna and a receiving circuit. Therefore, there are increasing needs for the enhancement of the characteristics of LNAs in order to improve the received signal quality by compensating for signal loss.

The latest generation process (TaRF11) makes it possible to significantly improve the characteristics of low noise amplifiers (LNAs). This new process offers additional enhancement to RF characteristics when compared with TaRF10 – the current generation SOI-CMOS process. A key parameter for these devices is their noise figure (NF) that compares the signal-to-noise ratio at the input and output.

TaRF11-based MOSFETs, intended for use in LNAs, achieved a minimum noise figure (NF) of 0.48 dB @ 8 GHz, an improvement of 0.3 dB compared to similar devices developed with TaRF10. In common with TaRF10, the TaRF11 process allows the LNA, RF switch and control circuit to be fabricated on a single chip.

Innovative RF switch ICs are developed using Toshiba’s TaRFSOI process in conjunction with the group production facilities (Japan Semiconductor Corporation), allowing new products to be brought to market swiftly.

As end-use technology evolves, Toshiba will continue to develop their process to meet the market needs, including the move from 5 GHz to 7 GHz planned in the smartphone arena. In addition, Toshiba plans to develop devices for 7 GHz to 10 GHz ultra-wide band (UWB) using the TaRFSOI process.

News Links

A new window will open