Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Keyword Search

Parametric Search

Stock Check & Purchase

Toshiba Launches MOSFET Gate Driver Switch Intelligent Power Devices

14th May 2020

Flexible solid-state switches are ideally suited to automotive ECU applications

Toshiba Launches MOSFET Gate Driver Switch Intelligent Power Devices

Toshiba Electronics Europe GmbH (“Toshiba") has launched two new gate driver switch intelligent power devices (IPDs).  Fully AEC-Q100 compliant, the TPD7106F and TPD7107F can be used to control the conduction and shut-off of currents being supplied to automotive electronic control units (ECUs), including junction boxes and body control modules. They are also suited to use in power distribution modules and semiconductor relays.

When combined with Toshiba’s low on-resistance N-channel automotive MOSFETs, such as the TPHR7904PB (40V/150A) or TPH1R104PB (40V/120A), the TPD7106F and TPD7107F IPDs can serve as high-side switches to control load current. These new solid-state devices are able to replace mechanical relays, thereby reducing the size and power consumption of automotive ECUs. As they have no moving parts, they are free from the contact wear issues associated with mechanical relays, thereby helping to significantly reduce maintenance costs.

The TPD7106F and TPD7107F have an array of enhanced functions that support the high reliability required by automotive ECUs. These include a self-protection function and various built-in diagnostic features (voltage abnormalities, over-current, over-temperature, reversed power connections, floating ground pin and short to VDD) that are output to the microcontroller. As a result, the new IPDs can monitor load operation as well as the MOSFET to which they are connected. Should abnormal operation occur, they can rapidly turn off the MOSFET to reduce the load current flowing through it - without the need for microcontroller intervention.

The new IPDs substantially reduce bill-of-materials (BoM) costs and component count as they each have a built-in voltage boosting circuit. Efficient operation is assured with a supply current as low as 5μA (max) for the TPD7106F and 3μA (max.) for the TPD7107F when in stand-by mode. The TPD7106F is supplied in a compact 16-pin SSOP package, while the TPD7107F is housed in a WSON10A package. Both operate over wide temperature ranges, with the TPD7107F supporting -40°C to +125°C and the TPD7106F covering -40°C to +150°C.  

Shipments of these new IPDs start today.

A new window will open