Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Keyword Search

Parametric Search

Stock Check & Purchase

Toshiba announces compact intelligent power device with 600V rating

28th May 2020

Efficient operation reduces power consumption of motor equipment

Toshiba announces compact intelligent power device with 600V rating

Toshiba Electronics Europe (“Toshiba”) has announced a high voltage intelligent power device intended for driving the motor within equipment such as air conditioners, air cleaners and pumps. With its rated power supply voltage (VBB) of 600V, the TPD4162F can be used for any applications with input signals in the range 200 to 220VAC.

The new IC contains a PWM circuit, 3-phase decoder, level shifting high-side driver and low side driver with embedded IGBTs and FRDs. This allows direct drive of brushless DC (BLDC) motors with square wave input signals from a Hall sensor or Hall IC without the requirement for a PWM controller IC.  

Based upon a new process, the TPD4162F offers reduced power dissipation of approximately 10% compared its predecessor (TPD4152F), reducing the power dissipation of motor drivers.  

Multiple protection features including current limit, over current protection (OCP), thermal shutdown and undervoltage lockout (UVLO) are built in thereby reducing the need for peripheral circuits. This, along with the small HSSOP31 surface mount package with a 17.5 x 11.9mm footprint and 2.2mm height, allows for compact designs including the ability to mount the driver circuitry directly to the motor.  

Mass production has started and the first shipments will be made today.

 

A new window will open