Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Keyword Search

Parametric Search

Stock Check & Purchase

Toshiba Launches Ultra-Low Current Consumption CMOS Operational Amplifier

27th October 2020

New device contributes to longer operating time for battery-powered equipment

Toshiba Launches Ultra-Low Current Consumption CMOS Operational Amplifier

Toshiba Electronics Europe GmbH (“Toshiba") has released a new CMOS operational amplifier featuring ultra-low current consumption to its product line-up.

Operational amplifiers have a multitude of uses including boosting weak signals from sensors. To support longer use between charges of battery-operated equipment, including IoT edge devices and other mobile devices such as handheld POS terminals they must also deliver lower current consumption.

Toshiba has used its CMOS process technology to optimize the circuitry of the new TC75S102F operational amplifier thereby lowering its power consumption to ultra-low levels. With a supply voltage between 1.5V and 5.5V, the new device is a full-range (rail-to-rail) input/output operational amplifier that offers higher performance than its predecessor. The supply current (IDD) will never exceed 0.6μA and is typically half that figure at just 0.27μA.

The new TC75S102F is supplied in a SOT-25 package measuring just 2.9mm x 1.6mm x 1.1mm. Shipments start today.

News Links

A new window will open