Select Product Categories
This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Toshiba HDDs in this website are shipped to OEM customers as storage devices installed in OEM PC systems. Please ask the PC manufacturer what kind of HDD will operate properly in the system. Consulting the PC manufacturer is recommended.
In addition to the physical dimensions and connectors, there are a lot of parameters (like power consumption, temperature distribution, etc.) that could differ. Also, older BIOS versions may have difficulties recognizing modern HDDs which exceed a certain storage capacity. So please contact your PC manufacturer or certified dealer for information on which HDDs can be used in your PC.