Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Keyword Search

Parametric Search

Stock Check & Purchase

Toshiba expands super junction N-Channel MOSFET series with addition of new 650V devices

24th June 2020

Enhanced FoM capabilities help to significantly boost power supply efficiency levels

Toshiba expands super junction N-Channel MOSFET series with addition of new 650V devices

Toshiba Electronics Europe GmbH (“Toshiba") has introduced eight new super junction N-channel power MOSFETs to strengthen its latest DTMOSVI series - which has already gained a lot of market traction thanks to an excellent ratio of on-resistance and support for elevated switching speeds.

The 650V-rated TK110N65Z, TK110Z65Z, TK110A65Z, TK125V65Z, TK155A65Z, TK170V65Z, TK190A65Z and TK210V65Z devices all possess highly appealing performance parameters. These MOSFETs present engineers with a 40% reduction in terms of their drain-source on-resistance x gate-drain charge (QGD) figure of merit (FoM) when compared to the previous DTMOS generation. As a consequence, they can raise the efficiency of switch-mode power supplies by approximately 0.36 % - thereby enabling a substantial decrease in switching losses, compared to the previous generation.

The new MOSFETs are targeted at use in the switch-mode power supplies of a broad range of industrial equipment (including data center infrastructure, back-up power sources and the power conditioners of photovoltaic generators). They will allow major performance upgrades when replacing existing devices. The TK110Z65Z, TK125V65Z, TK170V65Z and TK210V65Z offer a Kelvin source pin for improved control and efficiency increase potential. The TK110N65Z and TK110Z65Z fit into TO-247 packages with 3/4 pin’s, while the TK110A65Z, TK155A65Z and TK190A65Z come in fully isolated TO-220SIS packages. Finally, the TK125V65Z, TK170V65Z and TK210V65Z are all housed in an 8mm x 8mm DFN package format for surface mounting. This means DTMOSVI solutions can now be sourced whatever the specific board real estate requirements are.

Follow the link below for more information on Toshiba’s super junction N-Channel MOSFETs:

A new window will open