Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Keyword Search

Parametric Search

Stock Check & Purchase

Toshiba Introduces new Compact-Sized Photorelay Devices

15th September 2020

Optimized for high density implementations thanks to space-saving P-SON4 package

Toshiba Introduces new Compact-Sized Photorelay Devices
Toshiba Introduces new Compact-Sized Photorelay Devices

Toshiba Electronics Europe GmbH (“Toshiba") continues to drive innovation forward in optoelectronics with the addition of more photorelays to its expansive portfolio. All three of these devices are housed in the new P-SON4 package format. They are able to deliver very strong performance characteristics, while taking up significantly less board space than commonly used SOP packages.   

The TLP3480, TLP3481 and TLP3482 each have OFF-state output terminal voltage ratings and ON-state current ratings that are comparable to larger SOP-packaged devices - with these parameters ranging from 30V and 4.5A (for the TLP3480), 60V and 3A (TLP3481) to 100V and 2A (TLP3482). They also have low ON-resistance figures, due to incorporation of Toshiba’s proprietary trench MOSFET technology.

With 2.1mm x 3.4mm (typ.) dimensions, the new P-SON4 package format presents a very small mounting area. This means the photorelays are well suited to high-density board mounting, where there is very limited space available. Their 7.2mm2 (typ.) mounting area is approximately 74% smaller than 2.54SOP4 and 84% smaller than 2.54SOP6 package types.

These highly compact photorelay devices are intended for use in a wide variety of measuring equipment and instrumentation - with semiconductor testers, probe cards and I/O interface boards among the key applications deriving benefits.

A new window will open