December 18, 2017
Toshiba Electronic Devices & Storage Corporation
Expanding the line-up of the low-voltage U-MOS IX-H power MOSFET series
TOKYO— Toshiba Electronic Devices & Storage Corporation has today started to ship “TPH3R70APL” and “TPN1200APL,” new 100V additions to its low-voltage U-MOS IX-H N-channel power MOSFET series. The new devices are suitable for power supply applications in industrial equipment.
Fabricated with the company’s latest low-voltage U-MOS IX-H trench process, which optimizes the element structure, the TPH3R70APL and TPN1200APL deliver the industry’s lowest-in-class On-resistance[1]. In addition, compared with the current devices using the U-MOS VIII-H process, the new devices have lower “RDS(ON) × Qoss”, On-resistance times output charge, and “RDS(ON) × QSW”, On-resistance times gate switch charge, key figures of merit for MOSFETs for switching applications[2].
Toshiba Electronic Devices & Storage Corporation will continue to expand its MOSFET portfolio in line with market trends in order to help improve power supply efficiency.
(Unless otherwise specified, Ta=25℃)
Part number |
Absolute maximum ratings |
Drain-source On-resistance RDS(ON)max (mΩ) |
Total gate charge Qgtyp. (nC) |
Gate switch charge Qsw typ. (nC) |
Output charge Qoss typ. (nC) |
Input capacitance Cisstyp. (pF) |
Package | ||
---|---|---|---|---|---|---|---|---|---|
Drain- source voltage VDSS(V) |
Drain current (DC) ID @Tc = 25℃ (A) |
@VGS=10V | @VGS=4.5V | ||||||
100 |
90 | 3.7 | 6.2 | 67 | 21 | 74 | 4850 | SOP Advance | |
40 | 11.5 | 20 | 24 | 7.5 | 24 | 1425 |
TSON Advance
|
Notes:
[1] As of December 18, 2017 for MOSFETs with equivalent ratings. Toshiba Electronic Devices & Storage Corporation survey.
[2] TPH3R70APL has 10% lower RDS(ON) × Qoss than the U-MOSVIII-H series TPH4R10ANL.
TPH3R70APL has 10% lower RDS(ON) × QSW than the U-MOSVIII-H series TPH4R10ANL.
Follow the link below for more on MOSFET line-up.
Customer Inquiries:
Power Device Sales & Marketing Department
Tel: +81-3-3457-3933
*Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.