Toshiba Electronic Devices & Storage Corporation Launches New Series of Next Generation 10,500 RPM Enterprise Performance 2.5-inch HDD

December 19, 2017
Toshiba Electronic Devices & Storage Corporation

Offers maximum capacity of 2.4-terabyte

AL15SE Series

TOKYO— Toshiba Electronic Devices & Storage Corporation today announced the launch of AL15SE Series, the latest additions to its line-up of enterprise performance hard disk drives (HDD) for mission critical servers and storage systems. Sample shipments start today.

The AL15SE Series of 10,500RPM 2.5-inch[1] drives features a 12Gbits/s[2] SAS interface. A 4K native (4Kn) model and 512 emulation (512e) model, both featuring Advanced Format Sector Technologies, are available in 600-gigabytes (GB[3]), 900GB, 1.2-terabytes (TB), 1.8TB and 2.4TB capacities. A 2.4TB model offers approximately a 33% increase in maximum capacity from the 1.8TB of its predecessor in the AL14SE Series. The drives also deliver an approximately 15%[4] increase in the sustained data rate, pushing it to 260MiB/s[5]. These improvements in capacity and speed contribute to higher capacities and performance improvements in servers and storage systems.

The 512 native (512n) model optimized for legacy applications and hypervisor environment is available in 300GB, 600GB, 900GB and 1.2TB capacities.

Customers also can select models supporting Sanitize Instant Erase (SIE), which realizes fast invalidation of data recorded on the disks, allowing for efficient disposal and reuse.

Follow the link below for more on the new products and other enterprise HDDs.

Notes:

[1] "2.5-inch" describes the form factor of HDDs. They do not indicate drive's physical size.

[2] Read and write speed may vary depending on the host device, read and write conditions, and file size.

[3] Definition of capacity: We define a megabyte (MB) as 1,000,000 bytes, a gigabyte (GB) as 1,000,000,000 bytes and a terabyte (TB) as 1,000,000,000,000 bytes.  A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1GB = 230 = 1,073,741,824 bytes and therefore shows less storage capacity.  Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system, such as Microsoft Operating System and/or pre-installed software applications, or media content.  Actual formatted capacity may vary.

[4] Comparison with AL14SE (4Kn and 512e) transfer rate: 226 MiB/s

[5] A mebibyte (MiB) means 220, or 1,048,576 bytes, and a gibibyte (GiB) means 230, or 1,073,741,824 bytes.

Customer Inquiries:

Toshiba Electronic Devices & Storage Corporation

Storage Products Division

* Information in this document, including product prices and specifications, content of services and contact information, is correct on the date of the announcement but is subject to change without prior notice.

* Company names, product names, and service names mentioned herein may be trademarks of their respective companies.

A new window will open