March 29, 2018
Toshiba Electronic Devices & Storage Corporation
 
            
        
    TOKYO—Toshiba Electronic Devices & Storage Corporation ("Toshiba") today announced the launch of "TC78B025FTG," a three-phase brushless motor driver IC with a rotation speed control (closed loop control) function, for application in small fans used in home appliances and industrial equipment. Mass production will start from April.
The cooling fans used in servers and other must be small and rotate at high speeds with uniform accuracy. Uniformity is best achieved by using a speed-feedback method to suppress fluctuations in rotation speed caused by changes in power supply voltage and load. Until now, this has required the use of microcomputers, but Toshiba’s new solution achieves flexible rotation speed control without external microcomputers by incorporating a non-volatile memory (NVM). This also allows easy system configuration.
In addition, TC78B025FTG implements a 1-Hall drive system and current sense resistor-elimination system to reduce the number of external components and contribute to the space saving on boards. Industry-leading [1] low ON resistance (0.2Ω (typ.) (total of high and low sides)) reduces the IC’s self-heating during operation, so extending support to large current drives.
Rotation speed control uses the speed-feedback method to suppress rotation speed fluctuations caused by changes in power supply voltage and load. The IC’s non-volatile memory (NVM) supports a wide range of speeds, from hundreds to tens of thousands rotations per minute.
Mounting on the constricted board space of small fans is secured by adoption of a small package (4mm × 4mm). The 1-Hall drive and current detection resistor-free system (ACDS [2]) reduce external components.
Toshiba’s motor drive technology (InPAC [3]) realizes efficiency driving across a wide rotation range without adjustment burden. In addition, since the output ON resistance is as low as 0.2Ω (typ.), self-dissipation during IC operation can be reduced to achieve a high efficiency drive.
Cooling fans for servers, game machines, etc.
| Product name | TC78B025FTG | 
|---|---|
| Power supply | 4.5V to 16V | 
| voltage (Operating range) | 3.5A (Peak) | 
| Drive mode | Sine-wave drive; 150-degree commutation | 
| Other features | Output ON resistance (total of high and low sides): 0.2 Ω (typ.) | 
| Standby function | |
| Supports speed control by PWM signal input or analog voltage input | |
| Supports Hall element and Hall IC | |
| Error detection functions: thermal shutdown; over current protection; motor lock detection | |
| Package | VQFN24 (4mm×4mm×0.9mm) | 
Notes
[1] For IC used for 12V fan motors with a package size of 4 mm×4 mm. (As of March 29, 2018, Toshiba Electronic Devices & Storage Corporation survey.)
[2] Advanced Current Detection System: A current control method that does not require a sense resistor.
[3] Intelligent Phase Control: Toshiba’s new control technology that automatically adjusts the phase between the motor voltage and motor current, enabling efficient motor driving over a wide range of rotation speeds.
For further information on this new product, visit:
Customer Inquiries:
Mixed Signal IC Sales and Marketing Department
Tel: +81-44-548-2821
*Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.