News release / Products / Public Information
A new window will open
March 23, 2018
Toshiba Electronic Devices & Storage Corporation
TOKYO--Toshiba Electronic Devices & Storage Corporation (“Toshiba”) has released a dual MOSFET “SSM6N813R” with high ESD protection positioned for use in automotive applications, including as a driver IC for headlight LEDs, which require a high withstand voltage and a small footprint. Mass production shipments begin in April.
A maximum drain-source voltage (VDSS) of 100V ensures that SSM6N813R is suitable for headlight applications requiring multiple LEDs—a capability supported by high ESD immunity. Fabricated using the latest process and housed in a TSOP6F package, SSM6N813R has an allowable power dissipation of 1.5W and low on-resistance. In addition, the footprint of the TSOP6F package is 70% smaller than that of an SOP8 package.
(@Ta=25℃)
Items (Ta=25℃) |
SSM6N813R | ||
---|---|---|---|
Absolute maximum ratings | Drain-source voltage VDSS (V) |
100 | |
Gate-source voltage VGSS (V) |
±20 | ||
Drain current ID (A) |
3.5 | ||
Electrical Characteristics | Drain-source on-resistance RDS(ON) max (mΩ) |
VGS=10V | 112 |
VGS=4.5V | 154 | ||
Input capacitance Ciss typ. (pF) |
242 | ||
Package | TSOP6F | 2.9mm×2.8mm; t=0.8mm |
https://toshiba.semicon-storage.com/ap-en/product/mosfet/small-mosfet.html
Small Signal Device Sales & Marketing Department
Tel: +81-3-3457-3411
https://toshiba.semicon-storage.com/ap-en/contact.html
Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.