require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Company about
December 3, 2019
Toshiba Electronic Devices & Storage Corporation
TOKYO—Toshiba Electronic Devices & Storage Corporation ("Toshiba") today announced “TC78B009FTG,” a three-phase brushless motor control pre-driver IC that does not require Hall sensors, for applications that include high-speed fans used in servers, blowers, cordless vacuum cleaners, and robot vacuum cleaners. Mass production shipments start today.
In recent years, advances in server capacity and performance require larger and higher velocity fans for cooling the excess heat generated by the equipment. Similarly, blowers, vacuum cleaners and pumps also operate with high-speed impellers that require a power capability. Consequently, fan driver ICs need to be able to drive an external FET to deliver more power.
The new TC78B009FTG with sensorless control drives an external FET. It controls the gate driving current of an FET, and can be used with various FETs. In addition, a closed loop speed control regulates and maintains the motor rotational speed under dynamic power fluctuations and load variations. Precise setting of a speed profile is done by the built-in non-volatile memory (NVM) and TC78B009FTG therefore eliminates the need for an external MCU for closed loop speed control.
*Company names, product names, and service names may be trademarks of their respective companies.
Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.