require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Company about
April 28, 2020
Toshiba Electronic Devices & Storage Corporation
The introduction of Shingled Magnetic Recording (SMR) technology has enabled HDD manufacturers, such as Toshiba, to increase the capacity of their spinning platter drives beyond that of existing approaches. SMR technology is recognized as having an impact on write-speeds in drives where this technology is used, especially in the case of continuous random writing. For this reason, Toshiba products are carefully tailored to specific workloads and use cases.
For example, in use cases such as network-attached storage (NAS), where continuous random writing regularly occurs, Toshiba’s current product line for consumers features the N300, which does not use SMR.
The P300 / DT02 / DT02-V Desktop PC & Surveillance Hard Drive range of products, which are the product line for client drive application, such as all-in-one PCs, desktop PCs, and surveillance.
In the current range, the following drives do use SMR technology:
The L200 / MQ04 Laptop PC Hard Drive range of products,, which are the product line for client drive application, such as notebook PC, game consoles, and external enclosures, etc.
The following drives also use SMR technology:
Toshiba works extensively with Notebook and Desktop PC vendors on the selection of the appropriate storage media to help ensure the data integrity, reliability and planned lifetime requirements of the system. To find out more information on selecting the type of drive suitable for your needs, please visit consumer website at https://www.toshiba-storage.asia/
* Information in this document, including product prices and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement but is subject to change without prior notice.
* Company names, product names, and service names may be trademarks of their respective companies.