require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
October 30, 2020
Toshiba Electronic Devices & Storage Corporation
TOKYO—Toshiba Electronic Devices & Storage Corporation ("Toshiba") has launched the “TCR3RM Series” of 32 LDO regulators that bring enhanced power stabilization to DC power lines for mobile devices such as smartphones and wearable devices. Shipments of the first products in the series start today, and others will follow in turn.
The new TCR3RM series combines a bandgap circuit with a low-pass filter that allows through only extremely low frequencies, and a low-noise, high-speed operational amplifier, to realize an industry-leading[1] high ripple rejection ratio[2] and low output noise voltage.
The 32 products in the lineup have a maximum output current of 300mA and output voltages ranging from 0.9V to 4.5V. Customers can select output voltage by application.
The package is a compact DFN4C package, only 1mm x 1mm, suitable for camera applications, audio applications, and for the RF circuits of power supply lines in mobile devices requiring high-density mounting, such as smartphones and wearable devices.
In typical LDO regulators, when the frequency of noise on input voltage is over 1kHz, the ripple rejection ratio drops approximately 20dB for every 10 times increase in frequency. For noise over 100kHz, it drops approximately 40dB for every 10 times increase. As a result, the LDO regulator may not be sufficiently able to remove noise of over 100kHz generated by DC-DC converter circuits or similar circuits.
The new products offer an ample ripple rejection ratio and output noise voltage characteristics, even at noise frequencies of 100kHz or higher. This contributes to stabilization of power supply lines, including high output voltage accuracy.
Mobile devices
Part number |
TCR3RMxxA[3] |
||
---|---|---|---|
Package |
Name |
DFN4C |
|
Size typ. (mm) |
@Ta=25°C |
1.0×1.0, t=0.38 |
|
Operating ranges (@Ta= -40 to 85°C) |
Output current IOUT (mA) |
300 |
|
Output voltage VOUT (V) |
0.9 to 4.5 |
||
Input voltage VIN (V) |
1.8 to 5.5 |
||
Electrical Characteristics (Unless otherwise specified, @Tj=25°C) |
Output voltage VOUT min/max (mV) |
@VOUT<1.8V, Tj= -40 to 85°C |
-36/36 |
Output voltage VOUT min/max (%) |
@VOUT≥1.8V, Tj= -40 to 85°C |
-2/2 |
|
Quiescent current IB(ON) typ. (μA) |
@IOUT=0mA[4] |
7 |
|
Ripple rejection ratio R.R. typ. (dB) |
@f=1kHz, Ta=25°C |
100 |
|
@f=10kHz, Ta=25°C |
93 |
||
@f=100kHz, Ta=25°C |
68 |
||
@f=1MHz, Ta=25°C |
68 |
||
@f=2MHz, Ta=25°C |
67 |
||
Output noise voltage VNO typ. (μVrms) |
@IOUT=10mA, Ta=25°C |
5 |
|
Drop-out voltage VDO typ. (mV) |
@VOUT=2.8V, IOUT=300mA |
130 |
|
Load transient response ⊿VOUT typ. (mV) |
@IOUT=1mA→300mA |
-30 |
|
@IOUT=300mA→1mA |
30 |
||
Output voltage slew rate VOUTSR typ. (mV/μs) |
@VOUT=2.8V |
4 |
|
Sample Check & Availability |
Notes:
[1] Among LDO regulators with a maximum output of 300 mA, Toshiba survey as of October 28, 2020.
[2] The ripple rejection ratio (R.R. : Ripple rejection Ratio) is the same as the power supply rejection rate (PSRR: Power Supply Rejection Ratio) indicated on other manufacturers' products.
[3] 32 products. The number showing output voltage goes into "xx".
[4] Except control pull down current (ICT)
Follow the link below for more on the new products.
Follow the link below for more on Toshiba’s LDO regulators.
*Company names, product names, and service names may be trademarks of their respective companies.
*Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.