require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
September 21, 2021
Toshiba Electronic Devices & Storage Corporation
TOKYO--Toshiba Electronic Devices & Storage Corporation (“Toshiba”) has developed a model-based development (MBD) simulation technology that shortens verification times for automotive semiconductors by about 90 percent. [1] The technology allows automotive equipment developers to quickly evaluate designs using Toshiba’s automotive semiconductors, helping to shorten development times.
As electric vehicles grow in popularity and advanced driver-assistance systems become standard, automotive equipment is growing increasingly advanced and complicated. Model-based development, a development methodology that uses software to simulate models and evaluate performance in real-time, is helping product developers to refine complex design processes. In the automobile industry, MBD contributes to development advances by simultaneously progressing design and verification prior to making prototypes.
MBD separates functions into blocks and verifies total vehicle behavior by connecting each block. Detailed simulation models that include the behavior of semiconductors in individual blocks are required to verify heat and electromagnetic interference (EMI), essential parameters for assessing the performance of automotive equipment. However, as models become more detailed and precise, verification times are growing longer.
Toshiba took a long hard look at its current evaluation and verification technology for automotive equipment. Sub-systems like electric power steering comprise semiconductor-based electronic circuits that work in microseconds along with mechanical components, gears and shafts, that work in milliseconds. Toshiba’s current technology simulates the electronic circuits and mechanical components at the same time, on a microsecond basis, results in a large number of unnecessary and time-consuming calculations in the mechanical components. The technology is also complicated because it adopts the SPICE model—Simulation Program with Integrated Circuit Emphasis—that defines over 100 parameters for the simulation of semiconductor behavior.
Toshiba’s new modeling technology, “Accu-ROM™ ”, separately calculates the electronic circuits and the mechanical components. First it verifies the mechanical components, then simplifies the model for mechanical components and finally verifies the total system, including its electric circuits. This approach eliminates unnecessary calculations. In evaluating the electric circuits, the model automatically generates a Very High speed integrated circuit Hardware Description Language-Analog Mixed Signal (VHDL-AMS) model from the SPICE model. VHDL-AMS model allows the verification range to be limited to essential parameters, such as heat and EMI noise, shortening the verification time. For example, verification of a power steering system with Toshiba’s current technology takes 32 hours 51 minutes, but that falls to 3 hours 27 minutes[1] with the new technology.
Toshiba will use the new technology to promote development of high-heat dissipation and low noise automotive semiconductors, and to provide its customers with a development environment which makes it easier to use Toshiba’s products. In addition to automotive applications, Toshiba will use the new technology in semiconductors for other applications, such as industrial equipment and home appliances.
Notes
[1] Verification times for simulation of three-phase inverter circuits in an automotive electric power steering system during a right turn with a duration of six seconds.
<Updated on February 25, 2022: Added link to MBD article>
●Highlighted Contents:MBD (Model Based Development) using high-speed, high-precision thermal and noise simulation technology for automotive power semiconductor devices
* Accu-ROM™ is a trademark of Toshiba Electronic Device & Storage Corporation.
* All other company names, product names and service names may be trademarks of their respective companies.
Customer Inquiries:
*Company names, product names, and service names may be trademarks of their respective companies.
*Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.