February 7, 2023
Toshiba Electronic Devices & Storage Corporation
KAWASAKI, Japan—Toshiba Electronic Devices & Storage Corporation ("Toshiba") has launched two intelligent power devices that control the drive of the inductive loads of motors, solenoids, lamps and other devices used in applications such as the programmable logic controllers of industrial equipment. Shipments of the high-side switch (8-channels) “TPD2015FN” and the low-side switch (8-channels) “TPD2017FN” start today.
The new products use Toshiba’s analog device consolidation process (BiCD)[1] to achieve an on-resistance of 0.4Ω (typ.) in the output stage, over 50% lower than that of Toshiba’s current products[2]. Both TPD2015FN and TPD2017FN are housed in an SSOP30 package[3], which has a mounting area about 71% that of the SSOP24[4] package used for the current products[2], a height of 80% that of SSOP24 package, and a narrower, 0.65mm pin pitch. These improvements will help to reduce equipment size.
The maximum operating temperature of the new products is 110°C, higher than the 85°C of the current products[2], suiting them for operation in higher temperatures. In addition, both have built-in over current protection circuits and over temperature protection circuits, which help to improve equipment reliability.
Notes:
[1] Bipolar CMOS DMOS
[2] Toshiba’s current products: TPD2005F and TPD2007F
[3] SSOP30 package: 9.7 × 7.6 × 1.2mm (typ.)
[4] SSOP24 package: 13.0 × 8.0 × 1.5mm (typ.)
(Unless otherwise specified, Ta=25°C)
Part number | TPD2015FN | TPD2017FN | ||
---|---|---|---|---|
Package | SSOP30 | |||
Absolute maximum ratings |
Supply voltage VDD (V) | -0.3 to 40.0 | -0.3 to 6.0 | |
Input voltage VIN (V) | -0.3 to 6.0 | |||
VDDx - OUTx withstand voltage VDSS (V) | 50.0 | – | ||
Output withstand voltage VOUT (V) | – | 50.0 | ||
Output current IOUT (A) | Internally limited | |||
Power dissipation PD (W) | 1.8 | |||
Operating temperature Topr (°C) | -40 to 110 | |||
Junction temperature Tj (°C) | 150 | |||
Storage temperature Tstg (°C) | -55 to 150 | |||
Operating ranges | Operating supply voltage VDD(opr) (V) |
@Tj=25°C | 8 to 40 | 2.7 to 5.5 |
Electrical characteristics |
On resistance RDS(ON) typ. (Ω) |
@VDD=12V(TPD2015FN) / 5V (TPD2017FN), VIN=5V, IOUT=0.5A, Tj=25°C |
0.40 | |
Number of outputs | 8 | |||
Protection functions | Thermal shutdown | |||
Overcurrent shutdown | ||||
Sample Check & Availability | ![]() |
![]() |
Follow the link below for applications of TPD2017FN.
Customer Inquiries
Power Device Sales & Marketing Dept.
Tel: +81-44-548-2216
* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.