What is the definition of “allowable power dissipation”?

The allowable power dissipation is the maximum power dissipation permitted at up to the rated maximum junction temperature (Tj) of 150℃ when the ambient temperature, Ta, is 25℃. User should calcurate the derated allowable power dissipation because it should be decreased for higher ambient temperature.

A new window will open