require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Company about
2nd February 2021
Toshiba Electronics Europe GmbH (“Toshiba”) has further expanded its range of advanced eFuse ICs, with the introduction of the TCKE712BNL. This new device will ensure that the highest degrees of safety are always maintained. It is targeted at a broad spectrum of different consumer electronics goods - including cameras, cordless cleaner and power tools, cleaning robots, server, smart, speaker, thermostats and wireless chargers, etc.
While conventional fuses, such as glass tube and chip fuses, protect power supply lines by breaking if there is excessive current, eFuses provide a much more effective alternative. Unlike outdated conventional fuses, they are designed to support repeated use (being automatically reset by an internal logic signal). These devices also offer much faster responsiveness and have a greater breadth of built-in protection functions.
Exhibiting a 53mΩ on-resistance and with a trip time of only 320ns, the TCKE712BNL covers an input voltage range spanning from 4.4V to 13.2V. It is possible to adjust this device’s over-voltage threshold to fit with the specific application requirements. In addition, over-current (also adjustable), over-temperature and short-circuit protection mechanisms have all been included. A flag function transmits an external signal that will alert engineers of possible faults in the circuit design, so they can be addressed early on in the development process. Thanks to the reverse current blocking feature, there is the scope for this device to be employed in multiplexed systems.
Toshiba’s TCKE712BNL eFuse is supplied in a compact WSON10 package measuring just 3.00mm x 3.00mm, thereby taking up minimal board real estate.