require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Company about
11th March 2021
Toshiba Electronics Europe GmbH ("Toshiba") has announced five 650V superjunction power MOSFETs housed in the new compact SMD package in TO-leadless (TOLL) format. Measuring just 9.9mm x11.68mm x2.3mm (WxLxH), the TK065U65Z, TK090U65Z, TK110U65Z, TK155U65Z and TK190U65Z devices have a 27% smaller footprint than the conventional D2PAK package. Typical applications include server power supplies in data centres, solar (PV) power conditioners, uninterruptible power systems (UPS) and other industrial applications.
The lineup has been expanded to products in the DTMOS VI series with low On-resistance down to 65mΩ. In addition, the 4-pin package includes the option of a Kelvin source. This capability can reduce the parasitic inductance of the source wire in the package and enhance switching efficiency by suppressing oscillation. Compared to the TK090N65Z, a device with equivalent voltage and On-resistance that uses the TO-247 package without a Kelvin connection, the TK090U65Z has a 68% lower turn-on switching loss and turn-off switching loss is reduced by about 56%.
Deploying the latest generation of the DTMOS VI series of 650V superjunction power MOSFETs with the TOLL package will help engineers reduce the size of their end equipment and improve efficiency. DTMOS VI is targeting highest efficiency switching with best in class FOM: Rds(on) x Qdg.
The new devices enter mass production today and shipments begin immediately.