require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
10th August 2021
Toshiba Electronics Europe GmbH (TEE) announces the successful completion of compatibility testing between Toshiba’s new 18TB(1), 3.5-inch(2) MG09 Series and Microchip storage adapters. The operation of these hard disk drives (HDDs) is now confirmed on all common Adaptec® host bus adapters (HBAs) and redundant array of independent disk (RAID) adapters from Microchip.
HBAs and RAID adapters connect enterprise HDDs to the server, enabling the construction of advanced network architectures. Their smooth interplay ensures the functionality and operational stability of enterprise and cloud storage systems.
“We are very pleased that our long-term cooperation with Microchip made the qualification of the MG09 generation with their Smart Storage adapters so soon after the market launch. Companies using Adaptec adapters can install Toshiba's 18TB MG09 enterprise drives, for proven interoperability ,” says Rainer Kaese, Senior Manager Business Development Storage Products at TEE.
The confirmed compatibility of the MG09 Series refers to SAS 12GB/s MG09SCA18TE/A and the SATA 6GB/s versions MG09ACA18TE/A models. Tests were carried out on the new PCIe Gen 4 24G SAS/SATA/NVMe HBA and RAID tri-mode models, the HBA 1100 series, the SmartRAID 3100 series and the still widely used RAID predecessor, Series 8 . Not only were the basic functionality and compatibility of the interface checked, but hot-plug tests, power on tests and reboot tests were performed, as well Long-term stability was also confirmed via an extended duration test. The MG09 hard drives have thus qualified for entry on Microchip's compatibility list.
“Microchip’s latest generation of Adaptec NVMe and 24G SAS Tri-mode RAID and HBA storage adapters deliver the performance, connectivity, security, and ease of management our customers require in deploying new storage infrastructure,” said Jay Bennett, associate director of product management for Microchip’s data center solutions business unit. “Delivering solutions with demonstrated interoperability with ecosystem components like Toshiba’s SAS and SATA HDD products is vital in ensuring rapid and reliable integration and deployment of next generation storage solutions.”
The recently launched MG09 Series is based on Toshiba’s proprietary third-generation, 9-disk Helium-sealed design and incorporates game-changing flux control - microwave assisted magnetic recording (FC-MAMR) technology. With 12.5% more capacity than the previous 16TB models, the 18TB MG09 Series drives are compatible with the widest range of applications and operating systems.
Thorough compatibility testing conducted by Microchip follows on from tests that the company undertook on Toshiba’s Enterprise Capacity HDDs (models MG04 to MG08) and the Enterprise Performance HDD series (AL12 to AL15) in the past.
Follow the link below for more on the new 18TB Enterprise Capacity Hard Drive - MG09 Series: https://toshiba.semicon-storage.com/eu/storage/product/data-center-enterprise/cloud-scale-capacity/articles/mg09-series.html
Follow the link below for more on Toshiba’s HDDs line-up: https://toshiba.semicon-storage.com/eu/product/storage-products/enterprise-hdd.html
For more information on Adaptec products, please visit:
https://www.microchip.com/smartstorage
Notes:
[1] Toshiba defines a megabyte (MB) as 1,000,000 bytes, a gigabyte (GB) as 1,000,000,000 bytes and a terabyte (TB) as 1,000,000,000,000 bytes. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1TB = 240 bytes = 1,099,511,627,776 bytes and therefore shows less storage capacity. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system and/or pre-installed software applications, or media content. Actual formatted capacity may vary.
[2] "3.5-inch" means the form factor of HDDs. It does not indicate a drive's physical size
High Resolution Image (jpg)