24th June 2025
Toshiba Electronics Europe GmbH (“Toshiba”) starts sample shipment for the TB9M001FTG, the second product in the innovative Smart Motor Control Driver (SmartMCD™) series. This highly integrated device is specifically designed to deliver efficient and accurate control of brushed DC motors in automotive applications, including electric sunroofs, wipers, powered windows, and adjustable seats.
The SmartMCD™ TB9M001FTG integrates four low-side drivers that function as relay drivers, enabling forward and reverse control of two brushed DC motors when using single-pole double-throw (SPDT) relays. In addition, the device features a built-in microcontroller (MCU) with an Arm® Cortex®-M0 core, 192kB of Flash memory and an additional 16kB of Data Flash. It also includes two high-side drivers for supporting 5V and 12V loads to external components, a LIN-transceiver for in-vehicle communication, and a fully integrated power management system that generates all the required voltage levels from the car battery. All these functions are integrated into a compact VQFN48 package, measuring just 7mm x 7mm (typ.), enabling engineers to realise more compact system designs and reduce component count.
The TB9M001FTG is AEC-Q100 (Grade 1) qualified and meets ASIL-A requirements. It includes robust safety features such as built-in error detections for overcurrent (low-side driver, high-side driver), overvoltage, undervoltage, and thermal shutdown protection.
Sample shipments have commenced, with mass production of the SmartMCD TB9M001FTG scheduled for December 2025. Toshiba will continue expanding its lineup of SmartMCD series products for automotive DC and BLDC motor control applications.
Follow the link below for more on the new product.
TB9M001FTG
Follow the link below for more on Toshiba’s automotive motor drivers.
Analog Devices
* Arm and Cortex are registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
* SmartMCD™ is a trademark of Toshiba Electronic Devices & Storage Corporation.
* Other company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.