September 30, 2020
Toshiba Electronic Devices & Storage Corporation
TOKYO— Toshiba Electronic Devices & Storage Corporation ("Toshiba") has released a 12V, common-drain N-channel MOSFET “SSM6N951L” for the battery protection circuits in lithium-ion battery packs for mobile devices. Shipments start today.
Battery protection circuits in lithium-ion battery packs are required to feature extremely low resistance that reduces heat dissipation during charging and discharging, along with high density and high redundancy that improves the safety of the protection circuit itself. Achieving this requires MOSFETs that are small and thin, with very low On-resistance.
Toshiba has developed a dedicated micro process technology that excels in low On-resistance characteristics to meet emerging requirements such as quick charging. Applying this in SSM6N951L contributes to realizing a longer battery operating life by securing lower standby power consumption, due to low gate-source leakage current characteristics, along with lower power dissipation realized by industry-leading[1] low On-resistance characteristics.
Housed in a very small, thin chip scale package (CSP) (2.14x1.67mm t: 0.11mm (typ.)), the new MOSFET can be used in the limited, narrow mounting spaces characteristic of battery packs.
Toshiba will continue to develop products that are useful for such applications.
Devices with a lithium-ion battery pack
(@Ta=25℃)
Part number |
||
|---|---|---|
Configuration |
N-channel common-drain |
|
Absolute maximum ratings |
Source-source voltage VSSS (V) |
12 |
Gate–source voltage VGSS (V) |
±8 |
|
Source current (DC) IS (A) |
8 |
|
Gate-source leakage current IGSS max @VGS=±8V (μA) |
±1 |
|
Source-source On-resistance RSS(ON) typ. (mΩ) |
@VGS=4.5V |
4.4 |
@VGS=3.8V |
4.6 |
|
@VGS=3.1V |
4.9 |
|
@VGS=2.5V |
5.5 |
|
Package |
Name |
TCSP6A-172101 |
Size typ. (mm) |
2.14x1.67 t: 0.11 |
|
Sample Check & Availability |
||
Note:
[1] Comparison with the product of the same maximum rating, according to a survey by Toshiba as of September 29, 2020.
Follow the link below for more on the new product.
Follow the link below for more on Toshiba MOSFET line-up.
Customer Inquiries
Small Signal Device Sales & Marketing Department
Tel: +81-3-3457-3411
*Company names, product names, and service names may be trademarks of their respective companies.
*Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.