September 22, 2021
Toshiba Electronic Devices & Storage Corporation
TOKYO—Toshiba Electronic Devices & Storage Corporation ("Toshiba") has added “TB67S539FTG” to its lineup of stepping motor driver IC series that support constant current control, for office automation, commercial and industrial equipment. The new driver carries out constant current motor control without a current sense resistor.
TB67S539FTG incorporates Toshiba’s latest DMOSFET device[1], which allows it to realize a motor output voltage rating of 40V and a motor output current rating of 2.0A[2]. Use of a current detector for constant current motor control eliminates the need for an external current sense resistor. The H-bridge circuit for motor control has an Nch/Nch configuration, and a built-in charge pump circuit for output stage control. In addition, the new driver does not require the external capacitor that is generally used to drive the gates on the H-bridge, because it is incorporated in the product. This helps saving the space on printed circuit boards.
TB67S539FTG supports 4.5V to 34V motor drive power supplies, and can be used for applications driven by 24V, and in applications with 12V drivers, including surveillance cameras and projectors.
TB67S539FTG adopts a compact QFN32 package to reduce heat dissipation during use. Low On-resistance (upper + lower) between the output transistor drain and source, 0.8Ω (typ.), reduces heat generation.
Notes:
[1] As of September 2021.
[2] Actual driven motor current depends on the use environment and such factors as ambient temperature and power supply voltage.
(Unless otherwise specified, @Ta=25°C)
Part number |
|||||
|---|---|---|---|---|---|
Operating ranges |
Motor power supply |
@Ta=-20 to 85°C |
4.5 to 34 |
||
Absolute maximum ratings |
Motor output voltage VOUT (V) |
40 |
|||
Motor output current IOUT (A) |
2.0 |
||||
Supported motors |
Bipolar stepping motor |
||||
Output transistor between |
@VM=24V, |
0.8 |
|||
Power consumption IM1 max (μA) |
@sleep mode |
1 |
|||
Safety function |
Over-current detection, |
||||
Package |
Name |
QFN32 |
|||
Size (mm) |
5.0×5.0 |
||||
Sample Check & Availability |
|||||
Follow the links below for more on the new product.
Follow the link below for more on Toshiba’s motor driver ICs.
Customer Inquiries
* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.